Does G2D support Color space conversion from RGB to YUV?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does G2D support Color space conversion from RGB to YUV?

ソリューションへジャンプ
3,107件の閲覧回数
yongtang
Contributor I

Hi,freescale

  

   Does G2D support Color space conversion from RGB to YUV?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,860件の閲覧回数
art
NXP Employee
NXP Employee

Q. Does G2D support Color space conversion from RGB to YUV?

A. No, the RGB to YUV conversion is not supported by the GPU2D engine of the i.MX6 series processors. The only available output format for the GPU2D engine is RGB.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,861件の閲覧回数
art
NXP Employee
NXP Employee

Q. Does G2D support Color space conversion from RGB to YUV?

A. No, the RGB to YUV conversion is not supported by the GPU2D engine of the i.MX6 series processors. The only available output format for the GPU2D engine is RGB.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,860件の閲覧回数
saurabh206
Senior Contributor III

Hi art​

Does G2D support RGB24 to RGB565 conversion?

Does G2D support RGB24 to RGB24 scaling?

I also find that Horizontal flip is not working while RGB to RGB.

Horizontal flip is working while YUV to RGB.

Any updated document for G2D.

Thanks

Saurabh

0 件の賞賛
返信
2,860件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

According to the i.MX6 Graphics User's Guide, RGB and YUV formats can be set in source surface, but only RGB format can be set in destination surface.

0 件の賞賛
返信