Does G2D support Color space conversion from RGB to YUV?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does G2D support Color space conversion from RGB to YUV?

Jump to solution
3,108 Views
yongtang
Contributor I

Hi,freescale

  

   Does G2D support Color space conversion from RGB to YUV?

Labels (1)
0 Kudos
Reply
1 Solution
2,861 Views
art
NXP Employee
NXP Employee

Q. Does G2D support Color space conversion from RGB to YUV?

A. No, the RGB to YUV conversion is not supported by the GPU2D engine of the i.MX6 series processors. The only available output format for the GPU2D engine is RGB.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,862 Views
art
NXP Employee
NXP Employee

Q. Does G2D support Color space conversion from RGB to YUV?

A. No, the RGB to YUV conversion is not supported by the GPU2D engine of the i.MX6 series processors. The only available output format for the GPU2D engine is RGB.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,861 Views
saurabh206
Senior Contributor III

Hi art​

Does G2D support RGB24 to RGB565 conversion?

Does G2D support RGB24 to RGB24 scaling?

I also find that Horizontal flip is not working while RGB to RGB.

Horizontal flip is working while YUV to RGB.

Any updated document for G2D.

Thanks

Saurabh

0 Kudos
Reply
2,861 Views
jimmychan
NXP TechSupport
NXP TechSupport

According to the i.MX6 Graphics User's Guide, RGB and YUV formats can be set in source surface, but only RGB format can be set in destination surface.

0 Kudos
Reply