Does Android JB supports Dual Display?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does Android JB supports Dual Display?

1,583件の閲覧回数
teddy123
Contributor III

Hi Everyone,

I have a custom iMX6-solo board and am trying dual display on two LVDS showing different contents. Though LVDS can be operated in four modes namely split,dual,separate and single, I could get only mirror image of one lvds display over the other. Does Android OS recognizes two displays at a time ?

ラベル(4)
0 件の賞賛
返信
2 返答(返信)

1,422件の閲覧回数
saurabh206
Senior Contributor III

Hi,

teddy

Android Doesn't provide this feature.

You need to modified the Android frame works.

If you have specific content needs to run on 2nd display than it can be possible with minimal change.

Thanks

Saurabh

0 件の賞賛
返信

1,422件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Teddy123,

Which version of android BSP are you using? android_jb4.2.2_1.1.0-ga_source or android_jb4.3_1.0.0-ga_source?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信