Does Android JB supports Dual Display?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Android JB supports Dual Display?

1,597 Views
teddy123
Contributor III

Hi Everyone,

I have a custom iMX6-solo board and am trying dual display on two LVDS showing different contents. Though LVDS can be operated in four modes namely split,dual,separate and single, I could get only mirror image of one lvds display over the other. Does Android OS recognizes two displays at a time ?

Labels (4)
0 Kudos
Reply
2 Replies

1,436 Views
saurabh206
Senior Contributor III

Hi,

teddy

Android Doesn't provide this feature.

You need to modified the Android frame works.

If you have specific content needs to run on 2nd display than it can be possible with minimal change.

Thanks

Saurabh

0 Kudos
Reply

1,436 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Teddy123,

Which version of android BSP are you using? android_jb4.2.2_1.1.0-ga_source or android_jb4.3_1.0.0-ga_source?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply