Documentation for peripheral hardware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Documentation for peripheral hardware

Jump to solution
2,454 Views
hrishim
Contributor II

Is it possible to get documentation for the SD host controller on the iMX6 SABRE Smart Devices Board ? It would be useful when writing a driver (non-linux OS)

Thanks

Labels (2)
1 Solution
2,369 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hrishikesh

except IMX6DQCEC and IMX6DQRM

one can also look at iMX6_Firmware_Guide.pdf included in

i.MX 6Series Platform SDK  : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
2,370 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hrishikesh

except IMX6DQCEC and IMX6DQRM

one can also look at iMX6_Firmware_Guide.pdf included in

i.MX 6Series Platform SDK  : Bare-metal SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,368 Views
hrishim
Contributor II

Got the document. Just had to hit the expand all button

0 Kudos
Reply
2,368 Views
hrishim
Contributor II

Thank you for the response. I am unable to locate the Bare-metal SDK in that link. Could you post the direct link to the SDK or pdf file

0 Kudos
Reply