Documentation for iMX8M CSI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Documentation for iMX8M CSI

1,189 Views
d_brandt
Contributor I

Is there any new Information for the CSI-2 Interface in the iMX8M?

I want to interface an 1MP BW Sensor with the iMX8M and there are a number if questions the Reference Manual does not cover.

0 Kudos
Reply
1 Reply

1,131 Views
Yuri
NXP Employee
NXP Employee

Hello,

    Yes, it is  confirmed that details of the CSI I/F are missed in the Reference Manual (RM). 

Customers  may need wait for the next update of the RM.   I do not have exact schedule 

for new RM issue.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply