Documentation flat cable connector ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Documentation flat cable connector ?

24,908 Views
patrickklokowsk
Contributor I

Hello everyone,

i'm not able to find the right documentation for my type of board (png: picOfCon).

On

http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ

it is exactly my board illustrated. However the docu

http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS SCM-IMX6DQ?tab=Design_Tools_Tab

seems to refer to a version of the board with a different connector in that area where my flat cable connector is (png: wrong board).

On page 12 of the schematic pdf "SPF-28927-D" there is the pin configuration explained. But not for my kind of flat cable connector with 15 pins. On my board is a sticker with the following information "700-28927 REV X2 , SCH-28927 REV B3 , 04/14/16 35960-0093" if it helps. I would like to get the documentation of this board version (or just this connector).

Best regards

Patrick

Labels (2)
0 Kudos
Reply
5 Replies

24,725 Views
patrickklokowsk
Contributor I

Seems to be the MIPI 15 Pin CSIx camera interface?!

May somebody confirm that with a source.

0 Kudos
Reply

24,725 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Patrick,

Could you tell me if you  want to use the connector to realize some functions or something else?

Have a nice day

Rita

0 Kudos
Reply

24,727 Views
patrickklokowsk
Contributor I

Hi,

that's exactly the place where the wrong (other board version) documentation can be found.

0 Kudos
Reply

24,727 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Patrick,

I will do further confirming for you. And then give you reply.

Have a nice day

Rita

0 Kudos
Reply

24,727 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Patrick,

You can get all the infomations about the your board here http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ . Here if you mainly need the infromantions on the flat cable connector?
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply