Doc Bugs in Linux Ref Manual Rev. 1, 01/2017 Not corrected yet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Doc Bugs in Linux Ref Manual Rev. 1, 01/2017 Not corrected yet

1,467 Views
nagladhana
Contributor II

This was reported earlier by another user in release 3.14. That time it was told that the issue is highlighted to the documentation teams.

But these errors still not corrected in 4.1 upgrade. Created another thread to highlight the issue.

Device tree related stuff and the code locations should be thoroughly revised.

Good documentation is many times basis for selection of the SoC. iMX6 is well documented and the standard should be maintained. I refer to imx6 documents a lot and its pain to see things not done the right way even after being pointed to.

0 Kudos
Reply
3 Replies

1,389 Views
jimmychan
NXP TechSupport
NXP TechSupport

Could you tell me which document? and which page?

0 Kudos
Reply

1,389 Views
nagladhana
Contributor II

I mentioned the name of the document in my heading only. Its i.MX_Linux_Reference_Manual.pdf Rev 1, 01/2017. 

This one is the latest Linux reference manual.

There are references to plat-mxc which is non existent since 2 yrs. The references need to be correctde and old or removed file names need to be updated.

I could find these references at  Pg 39,Pg 128, Pg 151, Pg 320.

There's another post which had pointed out in 2015 :

https://community.nxp.com/thread/356996 

Hope to see them in errata or updated version soon.

0 Kudos
Reply

1,389 Views
jimmychan
NXP TechSupport
NXP TechSupport

Thanks for your reply. I will forward this to the corresponding person.

0 Kudos
Reply