Do you have a resolved or unresolved defects list for i.MX6 Android BSP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do you have a resolved or unresolved defects list for i.MX6 Android BSP?

2,156件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6 Android BSP.

Do you have a resolved & unresolved defects list for Android BSP(jb4.2.2_1.1.0-ga) same as ResolvedDefects.html in Linux BSP?

I read android release note in jb4.2.2_1.1.0-ga to check what defects are resolved from jb4.2.2_1.0.0-ga.

The update is written in chapter 6 "Change Lists", but it just a outline.

I want to get more information same as ResolvedDefects.html.

Best Regards,

Satoshi Shimoda

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,954件の閲覧回数
satoshishimoda
Senior Contributor I

Could you reply me?

0 件の賞賛
返信

1,954件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Satoshi San,

Basically the ResolvedDefects.html file that you find in the Linux BSP applies for Android BSP since it is based on the same kernel and hal files.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,954件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Jaime,

Yes, a part of issues are same as Linux BSP.

But there are some issues of android BSP specific also.

For example, ENGR00215165 is fixed by 2757-ENGR00215165-android-config-support-pptp-l2tp-vpn-fu.patch in android 4.2.2_1.1.0 BSP.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信

1,954件の閲覧回数
cliffhuang
Contributor II

Hi,

Where can I get the 2757-ENGR00215165-android-config-support-pptp-l2tp-vpn-fu.patch?

I have problem about use PPTP VPN in JB 4.2.2_r1 on IMX6 DL.

Best regards,

Cliff

0 件の賞賛
返信

1,954件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Cliff,

You can find it in /opt/android_jb4.2.2_1.1.0-ga_source/code/jb4.2.2_1.1.0-ga/kernel_imx.git directory if you decompress jb4.2.2_1.1.0-ga bsp to /opt.

Best Regards,

Satohsi Shimoda

0 件の賞賛
返信