Do Kernel logo and android bootanimation require IPU and GPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do Kernel logo and android bootanimation require IPU and GPU

3,236 Views
mrigendra_chaub
Contributor III

I have a sabresd reference board. I have few questions

I am using nxp provided android O source code. 

1. Does kernel logo showing needs IPU, PRE and PRG?

2. Does on android boot up, we need IPU, PRE and PRG?

3. Does on android boot up we need gpu to be working and it shouldn't be disabled when android home screens come up?

I am asking this because of I am not able to show kernel logo,

I have compiled test_fb_simple in android and on the shell if I do this,

sabre_6dq:/system/bin # ./test-fb-simple 24 10 10                             
vi.xres = 1920
vi.yres = 1080
vi.xresv = 1920
vi.yresv = 2160
vi.xoff = 0
vi.yoff = 0
vi.bits_per_pixel = 24
fi.line_length = 5760
[  171.373771] [dbg]: mxcfb_set_par
[  171.443976] imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
active buffer: 0
[  171.490114] [dbg]: mxcfb_set_par
[  171.597197] imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
active buffer: 1
[  171.610303] [dbg]: mxcfb_set_par
[  171.743963] imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
active buffer: 0

This is the bootup logs

2099200 bytes read: OK
hdr_size=124, bmp_bpix=16
[dbglcd]Display-bmp: 1920 x 1080 with 65536 colors, display 65536
[dbglcd]>>>>fb:0x17ef3900
[dbg]>>>CONFIG_BMP_16BPP
boota mmc0
not found VGA disp console.
kernel @ 14008000 (6106760)
ramdisk @ 15000000 (2038060)
fdt @ 14f00000 (65980)
## Booting Android Image at 0x11000000 ...
Kernel load addr 0x14008000 size 5964 KiB
Kernel command line: console=ttymxc0,115200 init=/init earlyprintk sabre_sku=0x20452221,0x3AA314,0x800FC6A5 video=mxcfb0:dev=ldb,fbpix=RGB565,bpp=16 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmode=name:custom,vmode:0,x:1920,y:1080,pclk:7365,le:50,ri:50,up:32,lo:2,hs:10,vs:2,sync:0 fbmem=base:397410304,size:4147200 cma=448M androidboot.hardware=freescale androidboot.console=ttymxc0 consoleblank=0 androidboot.selinux=permissive dmfc=3 buildvariant=userdebug androidboot.serialno=110f91d4ea9ac958 androidboot.soc_type=imx6qp androidboot.storage_type=sd gpt
## Flattened Device Tree blob at 14f00000
Booting using the fdt blob at 0x14f00000
Loading Kernel Image ... OK
Using Device Tree in place at 14f00000, end 14f131bb

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.17-g8dddd40-dirty (mrigendra.chaubey@CPU-384U) (gcc version 4.9.x 20150123 (prerelease) (GCC) ) #6 SMP PREEMPT Wed Jul 25 10:19:53 IST 2018
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt:Machine model: Freescale i.MX6 Quad Plus sabre Board
[ 0.000000] bootconsole [earlycon0] enabled
[ 0.000000] cma: early_cma(448M)
[ 0.000000] Reserved memory: created CMA memory pool at 0x7c000000, size 320 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] cma: dma_contiguous_reserve(limit ffffffff)
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] percpu: Embedded 14 pages/cpu @eef85000 s25984 r8192 d23168 u57344
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 522752
[ 0.000000] Kernel command line: console=ttymxc0,115200 init=/init earlyprintk sabre_sku=0x20452221,0x3AA314,0x800FC6A5 video=mxcfb0:dev=ldb,fbpix=RGB565,bpp=16 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmode=name:custom,vmode:0,x:1920,y:1080,pclk:7365,le:50,ri:50,up:32,lo:2,hs:10,vs:2,sync:0 fbmem=base:397410304,size:4147200 cma=448M androidboot.hardware=freescale androidboot.console=ttymxc0 consoleblank=0 androidboot.selinux=permissive dmfc=3 buildvariant=userdebug androidboot.serialno=110f91d4ea9ac958 androidboot.soc_type=imx6qp androidboot.storage_type=sd gpt
[ 0.000000] ##DEBUG:: This is sabre_setfbmode_dt
[ 0.000000] [dbg]sabre_setfbmode_dt,disp_intf: 10[ 0.000000] [dbg]sabre_setfbmode_dt,disp_intf: 10
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1736284K/2097152K available (8192K kernel code, 355K rwdata, 2676K rodata, 1024K init, 809K bss, 33188K reserved, 327680K cma-reserved, 983040K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB)
[ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB)
[ 0.000000] .data : 0xc0d00000 - 0xc0d58dd0 ( 356 kB)
[ 0.000000] .bss : 0xc0d58dd0 - 0xc0e23314 ( 810 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] L2C-310 erratum 769419 enabled
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[ 0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76470001
[ 0.000000] [DBG]before clk_set_rate
[ 0.000000] Switching to timer-based delay loop, resolution 333ns
[ 0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[ 0.008298] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[ 0.020813] Console: colour dummy device 80x30
[ 0.025383] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.035693] pid_max: default: 32768 minimum: 301
[ 0.040474] Security Framework initialized
[ 0.044683] SELinux: Initializing.
[ 0.048347] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.055081] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.062307] ##DEBUG11
[ 0.064748] ##DEBUG
[ 0.066988] ##DEBUG12
[ 0.069390] ##DEBUG
[ 0.072133] CPU: Testing write buffer coherency: ok
[ 0.077545] CPU0: update cpu_capacity 1024
[ 0.081744] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.087565] Setting up static identity map for 0x10100000 - 0x10100058
[ 0.293799] CPU1: update cpu_capacity 1024
[ 0.293807] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.373780] CPU2: update cpu_capacity 1024
[ 0.373788] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[ 0.453785] CPU3: update cpu_capacity 1024
[ 0.453792] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[ 0.453885] Brought up 4 CPUs
[ 0.486832] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[ 0.493114] CPU: All CPU(s) started in SVC mode.
[ 0.497879] CPU3: update max cpu_capacity 1024
[ 0.503484] devtmpfs: initialized
[ 0.503791] CPU2: update max cpu_capacity 1024
[ 0.530500] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.538840] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.548847] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.572429] pinctrl core: initialized pinctrl subsystem
[ 0.579354] NET: Registered protocol family 16
[ 0.591421] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.633446] cpuidle: using governor menu
[ 0.637852] CPU identified as i.MX6QP, silicon rev 1.0
[ 0.643093] ##This is function sabre_board_setup line 85 of file "/home/mrigendra.chaubey/CMAP/android_build/vendor/nxp-opensource/kernel_imx/arch/arm/mach-imx/mach-imx6q_sabre.c".
[ 0.659960] sabre_dt_overlay_named: applied 'fbmode'
[ 0.665159] sabre_dt_overlay_compat(sabre,Bluefin):
[ 0.670730] sabre_dt_overlay_compat: applied 'keypad_backlight_pwm1'
[ 0.677409] sabre_dt_overlay_compat: applied 'keypad_backlight_bluefin'
[ 0.684281] sabre_dt_overlay_compat: applied 'can_1'
[ 0.689474] sabre_dt_overlay_compat: applied 'can_2'
[ 0.694735] sabre_dt_overlay_compat: applied 'uart_2'
[ 0.700026] sabre_dt_overlay_compat: applied 'uart_3'
[ 0.705573] sabre_dt_overlay_compat: applied 'sc16is762-spi2'
[ 0.711611] sabre_dt_overlay_compat: applied 'usb'
[ 0.716724] sabre_dt_overlay_compat: applied 'ti_wifi_common'
[ 0.722773] sabre_dt_overlay_compat: applied 'kim_uart3'
[ 0.728551] sabre_dt_overlay_compat: applied 'ti_wifi_usdhc2_2'
[ 0.734742] sabre_dt_overlay_compat: applied 'eth-switch'
[ 0.740440] sabre_dt_overlay_compat: applied 'buzzer'
[ 0.745876] sabre_dt_overlay_compat: applied 'hdmi-1'
[ 0.751194] sabre_dt_overlay_compat: applied 'remotepower'
[ 0.757134] sabre_dt_overlay_compat: applied 'video_input_i2c3_mipi'
[ 0.763825] sabre_dt_overlay_compat: applied 'hdmi-mxcfb2'
[ 0.769599] sabre_dt_overlay_compat: applied 'hdmi-i2c2'
[ 0.775189] sabre_dt_overlay_compat: applied 'Bluefin'
[ 0.780535] sabre_dt_overlay_compat(sabre,Bluefin-1):
[ 0.786236] sabre_dt_overlay_compat: applied 'lcd_backlight_bluefin_16_19'
[ 0.793478] [DBG]NSKU_ETH_RMII
[ 0.796660] OF: overlay: of_build_overlay_info() failed for tree@/sabre-overlay/ethernet-rmii
[ 0.805395] sabre_dt_overlay_named: applied 'ethernet-rmii'
[ 0.811154] sabre_dt_overlay_named: of_overlay_create() failure status: -19
[ 0.818411] sabre_dt_link_gpios: mxcfb0 backlight-en-gpio[0] = gpio4-25
[ 0.825272] sabre_dt_link_gpios: tempmon cpu-fan-gpio[0] = gpio6-8
[ 0.831693] sabre_dt_link_gpios: power_btn gpios[0] = gpio1-21
[ 0.837762] sabre_dt_link_gpios: user_btn gpios[0] = gpio4-24
[ 0.843748] sabre_dt_link_gpios: mmc1 cd-gpios[0] = gpio1-8
[ 0.849552] sabre_dt_link_gpios: remotepower on-gpio[0] = gpio1-14
[ 0.855973] sabre_dt_link_gpios: remotepower off-gpio[0] = gpio1-22
[ 0.862465] sabre_dt_link_gpios: remotepower sense-gpio[0] = gpio5-16
[ 0.869147] sabre_dt_link_gpios: ecspi4 cs-gpios[0] = gpio2-20
[ 0.875224] sabre_dt_link_gpios: fec phy-reset-gpios[0] = gpio3-6
[ 0.881548] sabre_dt_link_gpios: wlan_en_reg gpio[0] = gpio2-18
[ 0.887698] sabre_dt_link_gpios: kim nshutdown_gpio[0] = gpio5-31
[ 0.894026] sabre_dt_link_gpios: ecspi2 cs-gpios[0] = gpio1-26
[ 0.900261] sabre_dt_link_gpios: gpio_keys enabled (2 buttons)
[ 0.906321] ##This is function sabre_board_setup line 339 of file "/home/mrigendra.chaubey/CMAP/android_build/vendor/nxp-opensource/kernel_imx/arch/arm/mach-imx/mach-imx6q_sabre.c". Done
[ 0.959678] imx6q_init_machine 1
[ 0.963612] In imx6q_enet_phy_init
[ 0.967751] No ATAGs?[ 0.969881] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.978019] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 1.045222] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 1.055132] imx-gpc 20dc000.gpc: Registered imx-gpc
[ 1.099044] mxs-dma 110000.dma-apbh: initialized
[ 1.106612] SCSI subsystem initialized
[ 1.110761] libphy: Generic PHY: Registered new driver
[ 1.116163] libphy: Generic 10G PHY: Registered new driver
[ 1.122055] usbcore: registered new interface driver usbfs
[ 1.127823] usbcore: registered new interface driver hub
[ 1.133406] usbcore: registered new device driver usb
[ 1.139947] i2c i2c-1: IMX I2C adapter registered
[ 1.144793] i2c i2c-1: can't use DMA, using PIO instead.
[ 1.151003] i2c i2c-2: IMX I2C adapter registered
[ 1.155845] i2c i2c-2: can't use DMA, using PIO instead.
[ 1.161502] media: Linux media interface: v0.10
[ 1.166288] Linux video capture interface: v2.00
[ 1.171191] pps_core: LinuxPPS API ver. 1 registered
[ 1.176288] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 1.185643] PTP clock support registered
[ 1.213446] [dbg]before ipu_disp_init ipu_probe
[ 1.218079] [dbg]ipu_dmfc_init
[ 1.221284] [dbg] _ipu_dmfc_init
[ 1.224636] imx-ipuv3 2400000.ipu: IPU DMFC ONLY-DP HIGH RESOLUTION: 5B(0~3), 5F(4~7)
[ 1.263446] [dbg]before ipu_disp_init ipu_probe
[ 1.268077] [dbg]ipu_dmfc_init
[ 1.271279] [dbg] _ipu_dmfc_init
[ 1.274634] imx-ipuv3 2800000.ipu: IPU DMFC ONLY-DP HIGH RESOLUTION: 5B(0~3), 5F(4~7)
[ 1.283585] imx-prg 21cc000.prg: [dbg]ipu_prg_probe
[ 1.288641] imx-prg 21cc000.prg: driver probed
[ 1.293230] imx-prg 21cd000.prg: [dbg]ipu_prg_probe
[ 1.298332] imx-prg 21cd000.prg: driver probed
[ 1.303206] imx-pre 21c8000.pre: [dbg]ipu_pre_probe
[ 1.308425] imx-pre 21c8000.pre: driver probed
[ 1.313015] imx-pre 21c9000.pre: [dbg]ipu_pre_probe
[ 1.318199] imx-pre 21c9000.pre: driver probed
[ 1.322784] imx-pre 21ca000.pre: [dbg]ipu_pre_probe
[ 1.327966] imx-pre 21ca000.pre: driver probed
[ 1.332556] imx-pre 21cb000.pre: [dbg]ipu_pre_probe
[ 1.337722] imx-pre 21cb000.pre: driver probed
[ 1.342785] Advanced Linux Sound Architecture Driver Initialized.
[ 1.350951] clocksource: Switched to clocksource mxc_timer1
[ 1.356775] VFS: Disk quotas dquot_6.6.0
[ 1.360856] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.385528] NET: Registered protocol family 2
[ 1.390680] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 1.397965] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 1.404667] TCP: Hash tables configured (established 8192 bind 8192)
[ 1.411279] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 1.417334] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 1.424025] NET: Registered protocol family 1
[ 1.428948] RPC: Registered named UNIX socket transport module.
[ 1.435000] RPC: Registered udp transport module.
[ 1.439802] RPC: Registered tcp transport module.
[ 1.444622] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.451470] Trying to unpack rootfs image as initramfs...
[ 1.587463] ##DEBUG: Freeing initrd memory: 1992K (c5000000 - c51f2000)
[ 1.595004] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[ 1.605392] Bus freq driver module loaded
[ 1.609822] sabre_hal driver module loaded
[ 1.614432] remotepower: io_input_at_start = 0
[ 1.618977] remotepower: state -> STARTUP
[ 1.623121] remotepower: io -> IN
[ 1.626670] remotepower driver module loaded
[ 1.632949] audit: initializing netlink subsys (disabled)
[ 1.638497] audit: type=2000 audit(1.610:1): initialized
[ 1.645245] workingset: timestamp_bits=30 max_order=19 bucket_order=0
[ 1.666052] Registering sdcardfs 0.1
[ 1.671351] NFS: Registering the id_resolver key type
[ 1.676530] Key type id_resolver registered
[ 1.680812] Key type id_legacy registered
[ 1.684992] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 1.698771] bounce: pool size: 64 pages
[ 1.703098] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 1.710605] io scheduler noop registered (default)
[ 1.716108] imx-weim 21b8000.weim: Driver registered.
[ 1.723441] pwm-backlight.0 supply power not found, using dummy regulator
[ 1.732780] keypad-pwm-backlight.0 supply power not found, using dummy regulator
[ 1.741048] ldb 2000000.aips-bus:ldb@020e0008: split mode
[ 1.746837] ldb 2000000.aips-bus:ldb@020e0008: split mode or dual mode, ignoring second output
[ 1.756922] 20e0000.hdmi_video supply HDMI not found, using dummy regulator
[ 1.764918] [dbg]:mxcfb_probe
[ 1.768050] mxc_sdc_fb fb@0: ##DEBUGmxc_ipuv3_fb.c::registered mxc display driver ldb
[ 1.776087] [dbg]: mxcfb_set_par
[ 1.776135] [dbg]:mxcfb_map_video_memory
[ 1.794348] Copying splash screen (fb_base=0xf0aa4000, fb_size=4147200, fb_stride=3840, ss_base=0xc7b00000, ss_size=4147200, ss_stride=3840)
[ 1.821385] [dbg]ipu_init_channel_buffer width:1920 height:1080
[ 1.821412] [dbg]ipu_init_channel_buffer1 width:1920 height:1080 dma_chan:23
[ 1.821413] [dbg]_ipu_dmfc_set_wait4eot
[ 1.821416] [dbg]_ipu_dmfc_set_wait4eot dma_chan 23
[ 1.821418] [dbg] _ipu_dmfc_init
[ 2.821982] imx-prg 21cc000.prg: wait for buffer ready timeout
[ 4.310937] imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
[ 4.536311] [dbg]mxcfb_register success
[ 4.540293] [dbg]: mxcfb_set_par
[ 4.540336] [dbg]:mxcfb_map_video_memory
[ 4.550804] [dbg]mxcfb_register success
[ 4.554876] [dbg]:mxcfb_probe
[ 4.557974] mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
[ 4.585652] [dbg]vfb_register success
[ 4.590863] ##DEBUG:: imx_serial_init
[ 4.594841] ##DEBUG::serial_imx_probe
[ 4.598696] ##DEBUG::serial_imx_probe_dt
[ 4.602976] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 28, base_baud = 5000000) is a IMX
[ 4.611780] console [ttymxc0] enabled
[ 4.611780] console [ttymxc0] enabled
[ 4.619197] bootconsole [earlycon0] disabled
[ 4.619197] bootconsole [earlycon0] disabled
[ 4.628480] ##DEBUG::serial_imx_probe
[ 4.632266] ##DEBUG::serial_imx_probe_dt
[ 4.636390] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 76, base_baud = 5000000) is a IMX
[ 4.645439] ##DEBUG::serial_imx_probe
[ 4.649199] ##DEBUG::serial_imx_probe_dt
[ 4.653342] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 77, base_baud = 5000000) is a IMX
[ 4.679125] brd: module loaded
[ 4.683280] zram: Added device: zram0
[ 4.690234] libphy: Fixed MDIO Bus: probed
[ 4.694493] libphy: SMSC LAN83C185: Registered new driver
[ 4.700014] libphy: SMSC LAN8187: Registered new driver
[ 4.705416] libphy: SMSC LAN8700: Registered new driver
[ 4.710761] libphy: SMSC LAN911x Internal PHY: Registered new driver
[ 4.717259] libphy: SMSC LAN8710/LAN8720: Registered new driver
[ 4.723367] libphy: SMSC LAN8740: Registered new driver
[ 4.728606] CAN device driver interface
[ 4.732700] 2090000.flexcan supply xceiver not found, using dummy regulator
[ 4.740807] flexcan 2090000.flexcan: device registered (reg_base=f13c0000, irq=35)
[ 4.748520] 2094000.flexcan supply xceiver not found, using dummy regulator
[ 4.756542] flexcan 2094000.flexcan: device registered (reg_base=f13c8000, irq=36)
[ 4.765618] 2188000.ethernet supply phy not found, using dummy regulator
[ 4.779113] pps pps0: new PPS source ptp0
[ 4.784657] fec 2188000.ethernet: fec_enet_mii_init 1111
[ 4.790541] libphy: phy_device_register[ 4.794450] libphy: ##DEBUGphy_probe:: SMSC LAN8710/LAN8720
[ 4.800039] ##DEBUG::smsc_phy_probe
[ 4.806220] libphy: fec_enet_mii_bus: probed
[ 4.811384] fec 2188000.ethernet eth0: registered PHC device 0
[ 4.817584] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 4.824189] ehci-pci: EHCI PCI platform driver
[ 4.828943] usbcore: registered new interface driver cdc_acm
[ 4.834635] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 4.842815] usbcore: registered new interface driver usb-storage
[ 4.850411] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 4.858785] 2184000.usb supply vbus not found, using dummy regulator
[ 4.869413] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 4.874349] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 4.910997] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 4.916682] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 4.923569] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 4.930803] usb usb1: Product: EHCI Host Controller
[ 4.935708] usb usb1: Manufacturer: Linux 4.9.17-g8dddd40-dirty ehci_hcd
[ 4.942440] usb usb1: SerialNumber: ci_hdrc.0
[ 4.947675] hub 1-0:1.0: USB hub found
[ 4.951500] hub 1-0:1.0: 1 port detected
[ 4.956280] 2184200.usb supply vbus not found, using dummy regulator
[ 4.966048] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 4.970991] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
[ 5.000975] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 5.006637] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 5.013464] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 5.020697] usb usb2: Product: EHCI Host Controller
[ 5.025618] usb usb2: Manufacturer: Linux 4.9.17-g8dddd40-dirty ehci_hcd
[ 5.032346] usb usb2: SerialNumber: ci_hdrc.1
[ 5.037515] hub 2-0:1.0: USB hub found
[ 5.041353] hub 2-0:1.0: 1 port detected
[ 5.046802] usbcore: registered new interface driver usbtouchscreen
[ 5.053761] i2c /dev entries driver
[ 5.059338] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=1)
[ 5.066999] device-mapper: uevent: version 1.0.3
[ 5.072212] device-mapper: ioctl: 4.35.0-ioctl (2016-06-23) initialised: [email protected]
[ 5.081715] sdhci: Secure Digital Host Controller Interface driver
[ 5.087905] sdhci: Copyright(c) Pierre Ossman
[ 5.092294] sdhci-pltfm: SDHCI platform and OF driver helper
[ 5.161024] mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
[ 5.231618] mmc0: host does not support reading read-only switch, assuming write-enable
[ 5.248913] mmc0: new high speed SDXC card at address aaaa
[ 5.265032] mmcblk0: mmc0:aaaa SC128 119 GiB
[ 5.278495] Primary GPT is invalid, using alternate GPT.
[ 5.283917] mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11
[ 5.331052] mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
[ 5.353714] sdhci-esdhc-imx 2194000.usdhc: card claims to support voltages below defined range
[ 5.380576] random: fast init done
[ 5.386331] mmc1: new high speed SDIO card at address 0001
[ 5.410994] mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[ 5.429705] mxc_vpu 2040000.vpu_fsl: VPU initialized
[ 5.437327] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[ 5.455035] caam 2100000.caam: ERA source: CAAMVID.
[ 5.462066] caam 2100000.caam: AXI pipeline throttling enabled.
[ 5.479284] caam 2100000.caam: Instantiated RNG4 SH1
[ 5.487353] caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4)
[ 5.493863] caam 2100000.caam: job rings = 2, qi = 0
[ 5.558849] mmc2: new DDR MMC card at address 0001
[ 5.574449] mmcblk2: mmc2:0001 M52516 14.3 GiB
[ 5.579380] mmcblk2boot0: mmc2:0001 M52516 partition 1 4.00 MiB
[ 5.585724] mmcblk2boot1: mmc2:0001 M52516 partition 2 4.00 MiB
[ 5.589558] caam algorithms registered in /proc/crypto
[ 5.598345] caam_jr 2101000.jr0: registering rng-caam
[ 5.604365] platform caam_sm: blkkey_ex: 4 keystore units available
[ 5.607320] mmcblk2rpmb: mmc2:0001 M52516 partition 3 4.00 MiB
[ 5.609194] mmcblk2: p1 p2
[ 5.619489] platform caam_sm: 64-bit clear key:
[ 5.624064] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 5.629736] platform caam_sm: 64-bit black key:
[ 5.634442] platform caam_sm: [0000] 43 98 1e 32 fe c1 cc 4a
[ 5.640115] platform caam_sm: [0008] be 87 7a e3 14 1b ef fa
[ 5.645803] platform caam_sm: 128-bit clear key:
[ 5.650432] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 5.656119] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 5.661808] platform caam_sm: 128-bit black key:
[ 5.666438] platform caam_sm: [0000] 17 83 62 d4 8d 2f df ed
[ 5.672169] platform caam_sm: [0008] 2a 6e 99 36 19 6a 42 d7
[ 5.677838] platform caam_sm: 192-bit clear key:
[ 5.682485] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 5.688153] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 5.693839] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[ 5.699505] platform caam_sm: 192-bit black key:
[ 5.704151] platform caam_sm: [0000] c4 8e 64 d7 16 a9 7e 46
[ 5.709821] platform caam_sm: [0008] 0f 8b 01 7a f3 b2 34 31
[ 5.715515] platform caam_sm: [0016] 09 20 e9 88 e4 00 95 02
[ 5.721206] platform caam_sm: [0024] b1 3b 0b 45 d1 fd 79 f8
[ 5.726872] platform caam_sm: 256-bit clear key:
[ 5.731516] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 5.737187] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 5.742874] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[ 5.748543] platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
[ 5.754227] platform caam_sm: 256-bit black key:
[ 5.758855] platform caam_sm: [0000] 40 26 b2 0c 29 0a 9e 2e
[ 5.764540] platform caam_sm: [0008] c1 e0 7b 70 1c d5 6c ef
[ 5.770209] platform caam_sm: [0016] 4b ac 87 6c 29 61 b4 53
[ 5.775895] platform caam_sm: [0024] 0a 33 a6 50 10 d7 ca c3
[ 5.781578] platform caam_sm: 64-bit unwritten blob:
[ 5.786553] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 5.792237] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 5.797905] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 5.803589] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 5.809257] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 5.814941] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 5.820609] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 5.826290] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 5.831976] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 5.837644] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 5.843339] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 5.849008] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 5.854690] platform caam_sm: 128-bit unwritten blob:
[ 5.859750] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 5.865436] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 5.871124] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 5.876792] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 5.882477] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 5.888145] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 5.893828] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 5.899496] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 5.905180] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 5.910848] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 5.916532] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 5.922214] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 5.927881] platform caam_sm: 196-bit unwritten blob:
[ 5.932959] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 5.938629] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 5.944314] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 5.949983] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 5.955670] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 5.961355] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 5.967023] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 5.972708] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 5.978375] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 5.984060] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 5.989728] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 5.995412] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 6.001094] platform caam_sm: 256-bit unwritten blob:
[ 6.006155] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 6.011874] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 6.017545] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 6.023232] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 6.028902] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 6.034589] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 6.040258] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 6.045943] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 6.051630] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 6.057298] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 6.062982] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 6.068650] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 6.074549] platform caam_sm: 64-bit black key in blob:
[ 6.079790] platform caam_sm: [0000] 8d 55 96 61 ac c2 d5 de
[ 6.085483] platform caam_sm: [0008] 95 40 d1 2f 93 a1 23 84
[ 6.091172] platform caam_sm: [0016] c7 45 f3 73 98 20 20 c3
[ 6.096842] platform caam_sm: [0024] 19 53 e7 07 3c e0 67 88
[ 6.102536] platform caam_sm: [0032] 90 a5 09 dc 8c 24 82 76
[ 6.108206] platform caam_sm: [0040] b0 9a 49 bb 08 7e 19 57
[ 6.113893] platform caam_sm: [0048] f2 f4 91 8d 56 86 2c 27
[ 6.119561] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 6.125245] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 6.130914] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 6.136599] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 6.142285] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 6.147951] platform caam_sm: 128-bit black key in blob:
[ 6.153291] platform caam_sm: [0000] 94 84 45 70 8e e7 34 bd
[ 6.158962] platform caam_sm: [0008] 55 4b ac 0f 9d ab e9 f4
[ 6.164648] platform caam_sm: [0016] 95 c3 8d 74 2f b8 a2 03
[ 6.170317] platform caam_sm: [0024] 8f 4d 99 20 ea 08 80 4e
[ 6.176003] platform caam_sm: [0032] 7b 18 e7 5a 8b c3 3e ec
[ 6.181688] platform caam_sm: [0040] 3e c5 56 7b 1a bc 3d 8f
[ 6.187357] platform caam_sm: [0048] 20 6e 15 6c f3 bb 5c 5e
[ 6.193043] platform caam_sm: [0056] e9 a9 0e e8 37 a7 be a8
[ 6.198711] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 6.204396] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 6.210064] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 6.215748] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 6.221428] platform caam_sm: 192-bit black key in blob:
[ 6.226751] platform caam_sm: [0000] 45 44 57 1f d3 ed 39 4b
[ 6.232438] platform caam_sm: [0008] 45 76 cd 9e cb 1b 68 8c
[ 6.238106] platform caam_sm: [0016] 24 47 72 fa 7b c9 b8 c5
[ 6.243791] platform caam_sm: [0024] a6 e3 8e 3c 26 f4 8f 30
[ 6.249460] platform caam_sm: [0032] b3 45 14 45 03 a3 8e ae
[ 6.255145] platform caam_sm: [0040] b9 1e e7 c1 1c a1 fc a8
[ 6.260813] platform caam_sm: [0048] 33 8c e8 12 93 81 3b 1a
[ 6.266499] platform caam_sm: [0056] fb ef 67 f4 83 8e 92 d3
[ 6.272186] platform caam_sm: [0064] ce b7 3f 28 8f 30 c1 ee
[ 6.277853] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 6.283537] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 6.289205] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 6.294886] platform caam_sm: 256-bit black key in blob:
[ 6.300210] platform caam_sm: [0000] ea 85 50 bf 6d 84 45 44
[ 6.305895] platform caam_sm: [0008] 18 a4 47 44 dd 34 0e 45
[ 6.311577] platform caam_sm: [0016] eb b5 22 0b 8b df 78 6a
[ 6.317245] platform caam_sm: [0024] b1 67 18 5a e0 e4 00 85
[ 6.322927] platform caam_sm: [0032] 75 32 4c 06 a7 55 73 7a
[ 6.328595] platform caam_sm: [0040] 4f b6 c4 27 15 c5 ec d6
[ 6.334281] platform caam_sm: [0048] 85 9a 0c b3 0f 79 01 3e
[ 6.339950] platform caam_sm: [0056] 7f 1e 5b 68 77 d1 1f 00
[ 6.345637] platform caam_sm: [0064] 01 88 de ac fb f3 9d 1f
[ 6.351322] platform caam_sm: [0072] 18 00 a2 1a 61 12 9d 25
[ 6.356990] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 6.362683] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 6.368553] platform caam_sm: restored 64-bit black key:
[ 6.373905] platform caam_sm: [0000] c5 4a 89 49 d7 0a c5 44
[ 6.379578] platform caam_sm: [0008] 0d d4 a3 ed 5d 42 bc 83
[ 6.385263] platform caam_sm: restored 128-bit black key:
[ 6.390672] platform caam_sm: [0000] 17 83 62 d4 8d 2f df ed
[ 6.396359] platform caam_sm: [0008] 2a 6e 99 36 19 6a 42 d7
[ 6.402043] platform caam_sm: restored 192-bit black key:
[ 6.407452] platform caam_sm: [0000] c4 8e 64 d7 16 a9 7e 46
[ 6.413139] platform caam_sm: [0008] 0f 8b 01 7a f3 b2 34 31
[ 6.418808] platform caam_sm: [0016] b4 da 00 f0 18 fe 65 3d
[ 6.424491] platform caam_sm: [0024] 68 8b fb 54 92 ee df 55
[ 6.430156] platform caam_sm: restored 256-bit black key:
[ 6.435581] platform caam_sm: [0000] 40 26 b2 0c 29 0a 9e 2e
[ 6.441266] platform caam_sm: [0008] c1 e0 7b 70 1c d5 6c ef
[ 6.446935] platform caam_sm: [0016] 4b ac 87 6c 29 61 b4 53
[ 6.452620] platform caam_sm: [0024] 0a 33 a6 50 10 d7 ca c3
[ 6.458602] snvs-secvio 20cc000.caam-snvs: can't get snvs clock
[ 6.464617] snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
[ 6.473459] hidraw: raw HID events driver (C) Jiri Kosina
[ 6.479144] usbcore: registered new interface driver usbhid
[ 6.484757] usbhid: USB HID core driver
[ 6.489070] ion_parse_dt_heap_common: id 0 type 4 name cma align 1000
[ 6.495917] ion_parse_dt_heap_common: id 1 type 1 name sys-contig align 1000
[ 6.503285] ion_parse_dt_heap_common: id 2 type 0 name system align 1000
[ 6.510760] ashmem: initialized
[ 6.515867] fsl-asrc 2034000.asrc: failed to get spba clock
[ 6.524091] NET: Registered protocol family 26
[ 6.528554] Netfilter messages via NETLINK v0.30.
[ 6.533950] xt_time: kernel timezone is -0000
[ 6.538505] Initializing XFRM netlink socket
[ 6.543509] NET: Registered protocol family 10
[ 6.548587] IPv6: [DBG]: ipv6_add_dev
[ 6.552426] IPv6: [DBG]: ipv6_add_dev
[ 6.556610] mip6: Mobile IPv6
[ 6.559614] ip6_tables: (C) 2000-2006 Netfilter Core Team
[ 6.565200] NET: Registered protocol family 17
[ 6.569676] NET: Registered protocol family 15
[ 6.574155] can: controller area network core (rev 20120528 abi 9)
[ 6.580421] NET: Registered protocol family 29
[ 6.585023] Key type dns_resolver registered
[ 6.591954] cpu cpu0: Registered imx6q-cpufreq
[ 6.597409] registered taskstats version 1
[ 6.616784] imx_thermal 2000000.aips-bus:tempmon: Automotive CPU temperature grade - max:125C critical:140C passive:125C
[ 6.629620] input: gpio-keys as /devices/soc0/gpio-keys/input/input0
[ 6.636758] OF: fdt:not creating '/sys/firmware/fdt': CRC check failed
[ 6.644461] wlan-en-regulator: disabling
[ 6.648396] ALSA device list:
[ 6.651394] No soundcards found.
[ 6.656628] ##DEBUG: Freeing unused kernel memory: 1024K (c0c00000 - c0d00000)
[ 6.667730] ##DEBUG
[ 6.669964] ##DEBUG
[ 6.673591] init: init first stage started!
[ 6.677954] init: First stage mount skipped (missing/incompatible fstab in device tree)
[ 6.686045] init: Skipped setting INIT_AVB_VERSION (not in recovery mode)
[ 6.692878] init: Loading SELinux policy
[ 6.711200] SELinux: Permission validate_trans in class security not defined in policy.
[ 6.719692] SELinux: the above unknown classes and permissions will be denied
[ 6.788565] audit: type=1403 audit(6.760:2): policy loaded auid=4294967295 ses=4294967295
[ 6.797061] selinux: SELinux: Loaded policy from /sepolicy
[ 6.797061]
[ 6.810022] selinux: SELinux: Loaded file_contexts
[ 6.810022]
[ 6.820142] init: init second stage started!
[ 6.836524] selinux: SELinux: Loaded file_contexts
[ 6.836524]
[ 6.843919] selinux: SELinux: Loaded property_contexts from /plat_property_contexts & /nonplat_property_contexts.
[ 6.843919]
[ 6.855732] init: Running restorecon...
[ 6.923690] selinux: SELinux: Could not stat /dev/block: No such file or directory.
[ 6.923690]
[ 6.933226] init: waitpid failed: No child processes
[ 6.938277] init: Couldn't load property file: Unable to open '/system/etc/prop.default': No such file or directory: No such file or directory
[ 6.951177] init: Couldn't load property file: Unable to open '/prop.default': No such file or directory: No such file or directory
[ 6.963753] init: Couldn't load property file: Unable to open '/odm/default.prop': No such file or directory: No such file or directory
[ 6.976046] init: Couldn't load property file: Unable to open '/vendor/default.prop': No such file or directory: No such file or directory
[ 7.005592] ueventd: ueventd started!
[ 7.009348] ueventd: Parsing file /ueventd.rc...
[ 7.015511] ueventd: Parsing file /vendor/ueventd.rc...
[ 7.020800] ueventd: Unable to open '/vendor/ueventd.rc': No such file or directory
[ 7.028522] ueventd: Parsing file /odm/ueventd.rc...
[ 7.033556] ueventd: Unable to open '/odm/ueventd.rc': No such file or directory
[ 7.041117] ueventd: Parsing file /ueventd.freescale.rc...
[ 7.052049] selinux: SELinux: Loaded file_contexts
[ 7.052049]
[ 7.166959] selinux: SELinux: Loaded file_contexts
[ 7.166959]
[ 7.236445] ueventd: Coldboot took 0.177867 seconds
[ 7.241177] ##DEBUG
[ 7.248915] audit: type=1400 audit(7.220:3): avc: denied { create } for pid=1 comm="init" name="cpu.rt_period_us" scontext=u:r:init:s0 tcontext=u:object_r:cpuctl_device:s0 tclass=file permissive=1
[ 7.267326] audit: type=1400 audit(7.240:4): avc: denied { write open } for pid=1 comm="init" path="/dev/cpuctl/cpu.rt_period_us" dev="tmpfs" ino=5318 scontext=u:r:init:s0 tcontext=u:object_r:cpuctl_device:s0 tclass=file permissive=1
[ 7.296695] ##DEBUG
[ 7.299019] watchdogd: watchdogd started (interval 10, margin 20)!
[ 7.322319] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: barrier=1
[ 7.573513] tune2fs: tune2fs 1.43.3 (04-Sep-2016)
[ 7.573513]
[ 7.581036] EXT4-fs (mmcblk0p10): Ignoring removed nomblk_io_submit option
[ 7.597197] EXT4-fs (mmcblk0p10): mounted filesystem with ordered data mode. Opts: errors=remount-ro,nomblk_io_submit
[ 7.875795] e2fsck: e2fsck 1.43.3 (04-Sep-2016)
[ 7.875795]
[ 7.881912] e2fsck: Pass 1: Checking inodes, blocks, and sizes
[ 7.881912]
[ 7.889237] e2fsck: Pass 2: Checking directory structure
[ 7.889237]
[ 7.896070] e2fsck: Pass 3: Checking directory connectivity
[ 7.896070]
[ 7.903178] e2fsck: Pass 4: Checking reference counts
[ 7.903178]
[ 7.909721] e2fsck: Pass 5: Checking group summary information
[ 7.909721]
[ 7.917112] e2fsck: userdata: 11/315120 files (0.0% non-contiguous), 55023/1260032 blocks
[ 7.917112]
[ 7.929928] EXT4-fs (mmcblk0p10): Ignoring removed nomblk_io_submit option
[ 7.942139] EXT4-fs (mmcblk0p10): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
[ 7.959004] EXT4-fs (mmcblk0p4): Ignoring removed nomblk_io_submit option
[ 7.971827] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
[ 7.993985] EXT4-fs (mmcblk0p9): mounted filesystem with ordered data mode. Opts: barrier=1
[ 8.118422] zram0: detected capacity change from 0 to 314572800
[ 8.182629] logd.auditd: start
[ 8.185761] logd.klogd: 8164791334
[ 8.190210] mkswap: Swapspace size: 307196k, UUID=abd5fd9b-2b9b-406e-8084-7bfb6e95a591
[ 8.200060] Adding 307196k swap on /dev/block/zram0. Priority:-1 extents:1 across:307196k SS
[ 8.362327] binder: 1436:1436 ioctl 620a 7b58bdb returned -22
[ 8.617787] IPv6: [DBG]: addrconf_qdisc_ok
[ 8.621957] IPv6: [DBG]qdisc_tx_is_noop returning false
[ 8.632020] logd.daemon: reinit
[ 8.837851] type=1400 audit(8.810:5): avc: granted { read } for pid=1 comm="init" name="ttymxc0" dev="tmpfs" ino=534 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 8.858864] type=1400 audit(8.810:5): avc: granted { read } for pid=1 comm="init" name="ttymxc0" dev="tmpfs" ino=534 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 8.877715] type=1400 audit(8.810:6): avc: granted { read open } for pid=1 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=534 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 8.900619] type=1400 audit(8.810:6): avc: granted { read open } for pid=1 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=534 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 8.924027] type=1400 audit(8.830:7): avc: granted { read } for pid=1510 comm="init" name="ttymxc0" dev="tmpfs" ino=534 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 8.943023] type=1400 audit(8.830:7): avc: granted { read } for pid=1510 comm="init" name="ttymxc0" dev="tmpfs" ino=534 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
[ 8.963262] type=1400 audit(8.830:8): avc: granted { read open } for pid=1510 comm="init" path="/dev/ttymxc0" dev="tmpfs" ino=534 scontext=u:r:init:s0 tcontext=u:object_r:tty_device:s0 tclass=chr_file
sabre_6dq:/ $ [ 9.091232] healthd: unable to get HAL interface, using defaults
[ 9.103164] healthd: No battery devices found
[ 9.107707] healthd: battery l=100 v=0 t=42.4 h=2 st=2 chg=a
[ 9.414595] healthd: battery l=100 v=0 t=42.4 h=2 st=2 chg=a

sabre_6dq:/ $
sabre_6dq:/ $
sabre_6dq:/ $ su
sabre_6dq:/ # [ 13.872974] init: starting service 'mediaextractor'...
[ 13.879177] init: Failed to make and chown /acct/uid_1040: Read-only file system
[ 13.886761] init: createProcessGroup(1040, 1644) failed for service 'mediaextractor': Read-only file system
[ 13.896767] init: property_set("ro.boottime.mediaextractor", "13857791668") failed: property already set
[ 13.906746] init: starting service 'wificond'...
[ 13.912625] init: Failed to make and chown /acct/uid_1010: Read-only file system
[ 13.920169] init: createProcessGroup(1010, 1645) failed for service 'wificond': Read-only file system
[ 13.929679] init: property_set("ro.boottime.wificond", "13891238668") failed: property already set
c[ 13.939170] init: starting service 'mediacodec'...
[ 13.945042] init: Failed to make and chown /acct/uid_1046: Read-only file system
sabre_6dq:/ # cd system//bin
sabre_6dq:/system/bin # [ 18.912599] init: starting service 'wificond'...
[ 18.918652] init: Failed to make and chown /acct/uid_1010: Read-only file system
[ 18.926244] init: createProcessGroup(1010, 1666) failed for service 'wificond': Read-only file system
[ 18.935760] init: property_set("ro.boottime.wificond", "18897190668") failed: property already set
[ 18.945430] init: starting service 'mediacodec'...
[ 18.951393] init: Failed to make and chown /acct/uid_1046: Read-only file system
[ 18.958959] init: createProcessGroup(1046, 1667) failed for service 'mediacodec': Read-only file system
[ 18.968735] init: property_set("ro.boottime.mediacodec", "18929927002") failed: property already set
[ 19.178737] init: Untracked pid 1671 exited with status 0
[ 19.191457] init: Service 'wificond' (pid 1666) killed by signal 6

sabre_6dq:/system/bin #
sabre_6dq:/system/bin # [ 20.576491] capability: warning: `main' uses 32-bit capabilities (legacy support in use)

sabre_6dq:/system/bin # [ 22.449229] random: crng init done
.[ 23.951307] init: starting service 'mediacodec'...
[ 23.957165] init: Failed to make and chown /acct/uid_1046: Read-only file system
[ 23.964847] init: createProcessGroup(1046, 1697) failed for service 'mediacodec': Read-only file system
[ 23.974573] init: property_set("ro.boottime.mediacodec", "23935788669") failed: property already set
/[ 24.143454] init: Untracked pid 1701 exited with status 0
[ 24.149311] init: Service 'wificond' (pid 1696) killed by signal 6
[ 24.158681] init: Sending signal 9 to service 'wificond' (pid 1696) process group...
[ 24.166660] init: Failed to open process cgroup uid 1010 pid 1696: No such file or directory
[ 24.175491] init: Error encountered killing process cgroup uid 1010 pid 1696: No such file or directory
[ 24.187219] init: Service 'mediacodec' (pid 1697) killed by signal 6
test_[ 29.130920] init: Untracked pid 1731 exited with status 0
[ 29.137427] init: Service 'wificond' (pid 1726) killed by signal 6
[ 29.144013] init: Sending signal 9 to service 'wificond' (pid 1726) process group...
[ 29.154275] init: Failed to open process cgroup uid 1010 pid 1726: No such file or directory
[ 29.163121] init: Error encountered killing process cgroup uid 1010 pid 1726: No such file or directory
[ 29.173636] init: Service 'mediacodec' (pid 1727) killed by signal 6
[ 29.180230] init: Sending signal 9 to service 'mediacodec' (pid 1727) process group...
[ 29.188886] init: Failed to open process cgroup uid 1046 pid 1727: No such file or directory
[ 29.197735] init: Error encountered killing process cgroup uid 1046 pid 1727: No such file or directory
[ 29.253779] init: Service 'mediaextractor' (pid 1725) killed by signal 6
sss
130|sabre_6dq:/system/bin #
130|sabre_6dq:/system/bin #
130|sabre_6dq:/system/bin # ./test_s[ 34.142279] init: Untracked pid 1747 exited with status 0
[ 34.148124] init: Service 'wificond' (pid 1742) killed by signal 6
[ 34.154507] init: Sending signal 9 to service 'wificond' (pid 1742) process group...
[ 34.162469] init: Failed to open process cgroup uid 1010 pid 1742: No such file or directory
[ 34.171034] init: Error encountered killing process cgroup uid 1010 pid 1742: No such file or directory
[ 34.181113] init: Service 'mediacodec' (pid 1743) killed by signal 6
[ 34.187520] init: Sending signal 9 to service 'mediacodec' (pid 1743) process group...
[ 34.195766] init: Failed to open process cgroup uid 1046 pid 1743: No such file or directory
[ 34.204638] init: Error encountered killing process cgroup uid 1046 pid 1743: No such file or directory
[ 34.259597] init: Service 'mediaextractor' (pid 1741) killed by signal 6
fb_[ 39.154029] init: Untracked pid 1763 exited with status 0
[ 39.159891] init: Service 'wificond' (pid 1758) killed by signal 6
[ 39.166290] init: Sending signal 9 to service 'wificond' (pid 1758) process group...
[ 39.174266] init: Failed to open process cgroup uid 1010 pid 1758: No such file or directory
[ 39.182813] init: Error encountered killing process cgroup uid 1010 pid 1758: No such file or directory
[ 39.192864] init: Service 'mediacodec' (pid 1759) killed by signal 6
[ 39.199266] init: Sending signal 9 to service 'mediacodec' (pid 1759) process group...
[ 39.207537] init: Failed to open process cgroup uid 1046 pid 1759: No such file or directory
[ 39.216102] init: Error encountered killing process cgroup uid 1046 pid 1759: No such file or directory
[ 39.254819] init: Service 'mediaextractor' (pid 1757) killed by signal 6

 

I get timeouts when trying to show a logo.

Also off the topic my android services are getting killed all the time.

As of now 

CONFIG_MXC_GPU_VIV=m

and it does not loads in kernel bootup.

If i make it y , I start getting vmalloc allocation failures.

So I am not getting how to get to show a logo in kernel and bootanimation.

Any debug points?

0 Kudos
Reply
1 Reply

1,882 Views
igorpadykov
NXP Employee
NXP Employee

Hi mrigendra

what board used in the case, if this is i.MX6QP (it is quite different from i.MX6Q)

then yes it may use IPU, PRE and PRG.

May be useful to look on logo patches :

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------