Display on IMXRT1176

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Display on IMXRT1176

2,868 次查看
Devaharsha
Contributor III

Hi, 

I have created three tasks using Free RTOS, out of which one of the tasks is using images to be displayed from the sd-card to the display. For this, I have modified SD_JPEG example. Additionally, I want other tasks to use PXP driver code which uses a manual input buffer. I am facing an issue in adding SD_JPEG example with PXP driver code.

Could you please help me with it? [I am using IMXRT 1176]

My issues are:

1) If I run PXP task and then if I run SD_JPEG task, there's display fluctuation. So, If I disable PS and AS at the end of PXP code, before running other tasks, will this work?

2) Another reason I think this can be because I am giving different buffers in both codes (g_frameBuffer and s_BufferLcd). If this is an issue how can I solve it?

3) Is it compulsory to use decoding format as same, as in SD_JPEG example its using RGB888 format and in PXP example its using RGB565 format?

 

Thanks,

Devaharsha

0 项奖励
回复
9 回复数

2,854 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Devaharsha ,

You can try to put buffer into noncacheable area.

PXP can support  RGB888 and RGB565 input.

 

Regards,

Jing

0 项奖励
回复

2,841 次查看
Devaharsha
Contributor III

Hi @jingpan,

I tried putting buffer in NonCacheble region -

Modified "SDK_ALIGN(static uint8_t g_frameBuffer[APP_FB_NUM][APP_FB_SIZE_BYTE], APP_FB_ALIGN);" to "AT_NONCACHEABLE_SECTION_ALIGN(static uint8_t g_frameBuffer[APP_FB_NUM][APP_FB_SIZE_BYTE], APP_FB_ALIGN));"

While compiling, it says "Cache is overflowed". I tried modifying value of RAM2 in properties option. But I am getting Bus Fault error. 

Is the above method correct or I am doing something wrong? Can you help me with this.

0 项奖励
回复

2,837 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Devaharsha ,

Obviously, OCRAM has not enough size for the buffer. You should split part of SDRAM to NCACHE_REGION.

 

Regards,

Jing

0 项奖励
回复

2,828 次查看
Devaharsha
Contributor III

Can you give an exact value of how much can be provided and exactly how to split RAM sizes in MCU IDE? 

0 项奖励
回复

2,822 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Devaharsha ,

Goto properties->MCU Settings

jingpan_0-1664430394950.png

 

0 项奖励
回复

2,812 次查看
Devaharsha
Contributor III

I have tried modifying RAM addresses as you have shown. There's no error in compiling.

1) First I am running sd_jpeg task, and it's working fine.

2) Then, I am running PXP driver, and it's working fine.

3) Again if the sd_jpeg task is getting run, I am getting PXP image and image from SD Card getting overlapped on the display. There's display fluctuation.

 

0 项奖励
回复

2,805 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

It seems the current display buffer is invaded when eLCDIF is reading it.

 

Regards,

Jing

0 项奖励
回复

2,793 次查看
Devaharsha
Contributor III

Is there any other way to run both PXP and JPEG SD code?

0 项奖励
回复

2,756 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Devaharsha ,

Sorry there isn't other examples.

 

Regards,

Jing

0 项奖励
回复