Display image from frame buffer /dev/fb0 to dual LCD i.MX8MMini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Display image from frame buffer /dev/fb0 to dual LCD i.MX8MMini

4,758 Views
rkhatal369
Contributor I

Hello Community,

We are using custom board based on i.MX8MMini. I am trying to display single image from frame buffer,  to dual LCD via MIPI-DSI interface. Can you please tell me how can i display single image on dual LCD.

For LCD selection i used MiPi switch. Please see attached diagram. From frame buffer i take single image and i want to display half part of image on LCD_1 and another half part of image on LCD_2.

Thank you!

Best Regards,

Rohit 

0 Kudos
Reply
5 Replies

4,734 Views
rkhatal369
Contributor I

Hello Community,

Please see below reference picture for LCD display.

I have to display image with half part on LCD_1 and another half part on LCD_2 like below picture.

lcds.png

We used mipi DSI and from frame buffer /dev/fb0 we want to display image on LCDs.

For LCD selection with higher rate (speed)  we used MIPI switch.

Any suggestion, Documents will be helpful.

Thank you!

Best regards,

Rohit

 

0 Kudos
Reply

4,719 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rohit

 

are both LCDs identical ?

For frame buffer may be useful to look at unit tests:

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_fb_test?h=imx_5.4.47_2.2.0

 

Best regards
igor

0 Kudos
Reply

4,707 Views
rkhatal369
Contributor I

Hello Igor, 

Thank you for reply,

Yes both LED's are identical.

Best regards,

Rohit

 

0 Kudos
Reply

4,738 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rohit 

 

could you provide more details about dual lcd connection, as in attached diagram

there is no "MiPi switch".  It is not possible just to connect two LCDs directly to MIPI-DSI module.

Dual LCD is easy to implement with i.MX8MQ connecting DCSS to HDMI and eLCDIF to MIPI-DSI.

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mq-evk-d...

However for i.MX8M Mini, which has not DCSS and HDMI I am not sure that it is feasible.

 

Best regards
igor

0 Kudos
Reply

4,722 Views
rkhatal369
Contributor I

Hello Igor,

Thank you for your reply.

Below are the LCD's connections details,

LCD_1 :

led_1.jpeg

LCD_2:

led_2.jpeg

MIPI Switch :

switcher.jpeg

At a time only one LCD will be selected using MIPI switch. But switching would be fast so user will be able to see data on both the screens.

Below is the flow diagram,

flow.jpeg

From Frame buffer we have to take image and via MIPI DSI we have to passes that image. Using MIPI Switch We select one of the LCD at time and display that image.

I do not understand how to pass half part of image on LCD_1 and another half part on LCD_2 from frame buffer.

Thank you!

Best regards,

Rohit 

 

0 Kudos
Reply