Display boot messages on hdmi/vga then ubuntu desktop on imx6q sabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Display boot messages on hdmi/vga then ubuntu desktop on imx6q sabresd

1,301件の閲覧回数
sumeetdube
Contributor III

Hi,

I want to display boot messages on hdmi/vga till the rootfs is mounted and then the desktop of ubuntu on my imx6q sabresd like custom board just like it happens on raspberry pi.

Can anybody help? I have used oneiric ubuntu rootfs from freescale and curretly boot messages are displayed on ttymxc1 console.

1 返信

1,072件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

You can try to set a different console in the u-boot bootargs.

For example I tried this with the fsl-image-gui image generated with Yocto.

setenv mmcargs 'setenv bootargs console=ttymxc3,${baudrate} console=tty1,${baudrate} ${smp} root=${mmcroot}'

And  see the bootlogs in the LVDS display and the UART console.

Best Regardds,

Alejandro

0 件の賞賛
返信