lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mtdblock0 31:0 0 32M 0 disk
mmcblk2 179:0 0 29.1G 0 disk
|-mmcblk2p1 179:1 0 83.2M 0 part
`-mmcblk2p2 179:2 0 1.5G 0 part /
mmcblk2boot0 179:32 0 4M 1 disk
mmcblk2boot1 179:64 0 4M 1 disk
i need to add 29G to / mount point i have added it using fdisk command and my lsblk is now showing
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mtdblock0 31:0 0 32M 0 disk
mmcblk2 179:0 0 29.1G 0 disk
|-mmcblk2p1 179:1 0 83.2M 0 part
`-mmcblk2p2 179:2 0 29G 0 part /
mmcblk2boot0 179:32 0 4M 1 disk
mmcblk2boot1 179:64 0 4M 1 disk
29G is mounted with root but when i give df -h
df -h
Filesystem Size Used Avail Use% Mounted on
/dev/root 1.4G 877M 440M 67% /
devtmpfs 2.3G 0 2.3G 0% /dev
tmpfs 2.8G 0 2.8G 0% /dev/shm
tmpfs 1.1G 9.1M 1.1G 1% /run
tmpfs 4.0M 0 4.0M 0% /sys/fs/cgroup
tmpfs 2.8G 60K 2.8G 1% /tmp
tmpfs 2.8G 16K 2.8G 1% /var/volatile
tmpfs 562M 4.0K 562M 1% /run/user/0
what i am missing to add the storage for the device is this the right approach to allocate memory for the system
已解决! 转到解答。