Disk Partition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disk Partition

1,450件の閲覧回数
1990rahulreddy
Contributor IV

I am following, "i.MX 6Dual/6Quad SABRE-SD Linux User's Guide, Rev. L3.0.35_4.1.0, 09/2013", In this they have given 16384 [starting at offset sector #16384, But It shows mi following error. Any Help ...My target is run OpenCv on this Board & Linaro ALIP is available for this. or Is there any way to install openCV & Ubuntu..in L3.14.28_1.0.0.

.sdcard    require no partition,But, I have to Install Ubuntu, so I am following this Document.

ラベル(2)
0 件の賞賛
返信
1 返信

1,127件の閲覧回数
b36401
NXP Employee
NXP Employee

It seems the log was actually not attached to the message.

So I can provide only common recomendation.

Please refer 4.3.3 Partitioning the SD/MMC card chapter of i.MX Linux User's Guide.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信