Disabling SDHC write protection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disabling SDHC write protection

6,678件の閲覧回数
vishakh
Contributor III

Hi All,

I am using i.MX6q custom board with Linux 3.0.35.

When I try to copy/create files to SDHC card, I am getting, "Read-only file system" message.

I tried disabling the write protection pin, but still facing the same issue. In the boot loader it works fine.

Below is the board file information:

static const struct esdhc_platform_data mx6_sd3_data __initconst = {

    .cd_gpio = MX6_SD3_CD;

    //.wp_gpio = MX6_SD3_WP;

    .always_present = 0;

    //.support_18v = 1;

    .keep_power_at_suspend = 1;

    .support_8bit = 1;

    .delay_line = 0;

    .cd_type = ESDHC_CD_CONTROLLER;

};

Please help me to solve this issue.

With Regards,

Vishakh

0 件の賞賛
返信
9 返答(返信)

6,174件の閲覧回数
danwei_luo
NXP Employee
NXP Employee

Hi Vishakh,

Are you  currently booting and loading file system from this SDHC card? If that is the case, then you can check your u-boot bootargs.

If it has following agrs:

"root=/dev/mmcblk2p2 rootwait ro"

Then you can change the "ro" to "rw" to make it writable.

Best regards,

Danwei Luo

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,174件の閲覧回数
vishakh
Contributor III

Hi Danwei Luo,

I am not using SDHC for booting purpose.

Thanks and Regards,

Vishakh

0 件の賞賛
返信

6,174件の閲覧回数
bandarulavanya
Contributor V

Hi Vishakh M,

From where you are trying to copy files from PC to sdcard or in board from one folder to another .

Thanks ,

Lavanya

0 件の賞賛
返信

6,174件の閲覧回数
vishakh
Contributor III

I am trying to copy files in board.

Regards,

Vishakh

0 件の賞賛
返信

6,174件の閲覧回数
bandarulavanya
Contributor V

Hi Vishakh M,

check once in your rootfs.

/etc/default# vi rcS  in this file.

# Indicate whether the rootfs is intended to be read-only or not.

# Setting ROOTFS_READ_ONLY to yes and rebooting will give you a read-only rootfs

# Normally you should not change this value.               

ROOTFS_READ_ONLY=no

thanks ,

lavanya

0 件の賞賛
返信

6,174件の閲覧回数
vishakh
Contributor III

Hi bandarulavanya​,

Thanks for the suggestion. ROOTFS_READ_ONLY is not set to 'yes'.

I found out that, in function mmc_blk_alloc_req of driver drivers/mmc/card/block.c, md->read_only is getting set.

But, I am not able to find out why this is being set. Any idea about this?

Also, we are using 4bit SDHC card in 8bit mode.

Thanks and Regards,

Vishakh

0 件の賞賛
返信

6,174件の閲覧回数
bandarulavanya
Contributor V

Hi Vishakh M,

have you checked your u boot boot args in that u r passing like

"mmcroot = /dev/mmcblkXpY rootwait ro " like this or  "mmcroot = /dev/mmcblkXpY rootwait rw "

Thanks & Regards,

Lavanya

0 件の賞賛
返信

6,174件の閲覧回数
vishakh
Contributor III

Hi bandarulavanya​,

In boot args "rw" is set. And we are not using SDHC card to mount file system.

Further, micro SD card and eMMC are working fine and we are even able to mount file system.

Thanks and Regards,

Vishakh

0 件の賞賛
返信

6,174件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vishakh

one can look at emmc configuration, it is used on sabresd board as sd4,

it also has not cd,wp signals. One can check with oscilloscope wp protection signal.

Could you try with official nxp sources

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files

linux-2.6-imx.git - Freescale i.MX Linux Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信