DirectFB Build Failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DirectFB Build Failed

2,123 Views
KrishnaPavan
Contributor II

Hi,

I am working with i.MX5X EVK and i have selected DirectFB package and tried to build LTIB.

But, It has thrown an error.

Processing: DirectFB
======================
Build path taken because: no prebuilt rpm,
Testing network connectivity
No network download connection available

Can't get: DirectFB-1.1.0.tar.gz at ./ltib line 790.


f_buildrpms() returned an error, exiting
traceback:
 main:560

These packages failed to build:
DirectFB

Build Failed

Please Suggest!

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,746 Views
KrishnaPavan
Contributor II

After installing some other packages, again the build fails

Processing: amd-gpu-bin-mx51
==============================
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/krishna/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' amd-gpu-bin-mx51 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/krishna/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/krishna/ltib/rpm/RPMS/arm/amd-gpu-bin-mx51-10.11.01-1.arm.rpm
error: failed dependencies:
    libc.so.6(GLIBC_2.11)   is needed by amd-gpu-bin-mx51-10.11.01-1

f_buildrpms() returned an error, exiting
traceback:
 main:560

Build Failed
Exiting on error or interrupt

This is the log I get,

However libc is available, but still the compilation throws an error!   Which, I dont know why?

Any comments on the cause and/or resolving of error are welcome

Please Suggest me!

0 Kudos
Reply

1,746 Views
methew
Contributor I

Have u fixed this problem???

0 Kudos
Reply