Direct Camera Input using HDMI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Direct Camera Input using HDMI

1,440件の閲覧回数
wildpossum
Contributor I

Hi All.

The HDMI standard has connectability for video output and input in its specification.

Thence I ordered the additional MCIMX-HDMICARD board part (24bit HDMI MX535/08) to supplement my MX53 Quick Start EVB.

If the board vendor has connected these pins and allows user to use them is also a matter of interest.

So, my questions to those knowledgeable on such matters -

Can I connect and use a digital camera output directly to the HDMI connector (as video input) ? 

If so, what functionality is available on-board for such usage?

Much thanks.

Grahame

タグ(1)
0 件の賞賛
返信
1 返信

1,220件の閲覧回数
sidebranch
Contributor II

Grahame,

I am very sure this option is not available on the HDMICARD (and the way it is connected to the i.MX53 video output only).

If you require a commercial HDMI to CSI (Camera Sensor Interface) solution, there might be converter boards for that.

Regards,

Leon.

0 件の賞賛
返信