Direct Camera Input using HDMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Direct Camera Input using HDMI

1,498 Views
wildpossum
Contributor I

Hi All.

The HDMI standard has connectability for video output and input in its specification.

Thence I ordered the additional MCIMX-HDMICARD board part (24bit HDMI MX535/08) to supplement my MX53 Quick Start EVB.

If the board vendor has connected these pins and allows user to use them is also a matter of interest.

So, my questions to those knowledgeable on such matters -

Can I connect and use a digital camera output directly to the HDMI connector (as video input) ? 

If so, what functionality is available on-board for such usage?

Much thanks.

Grahame

Tags (1)
0 Kudos
Reply
1 Reply

1,278 Views
sidebranch
Contributor II

Grahame,

I am very sure this option is not available on the HDMICARD (and the way it is connected to the i.MX53 video output only).

If you require a commercial HDMI to CSI (Camera Sensor Interface) solution, there might be converter boards for that.

Regards,

Leon.

0 Kudos
Reply