Digital IO voltages PF3000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Digital IO voltages PF3000

1,080 次查看
maartengeurts
Contributor I

In the datasheet of the PF3000 is the Vol max = 0.4*Vddio. When Vddio = 3.3V the Vol max is 1.32V and this is really high. in comparison to PF2000 is the Vol max 0.4V. is the 0.4V*Vddio correct because i will use the i.MX6SX connected to the PF3000?

标签 (2)
0 项奖励
回复
1 回复

996 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello

>>is the 0.4V*Vddio correct because i will use the i.MX6SX connected to the PF3000?

Yes, it is. Don't worry about it. It doesn't affect your application.


Have a great day,
TIC   Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复