Digital IO voltages PF3000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Digital IO voltages PF3000

416件の閲覧回数
maartengeurts
Contributor I

In the datasheet of the PF3000 is the Vol max = 0.4*Vddio. When Vddio = 3.3V the Vol max is 1.32V and this is really high. in comparison to PF2000 is the Vol max 0.4V. is the 0.4V*Vddio correct because i will use the i.MX6SX connected to the PF3000?

ラベル(2)
0 件の賞賛
返信
1 返信

332件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello

>>is the 0.4V*Vddio correct because i will use the i.MX6SX connected to the PF3000?

Yes, it is. Don't worry about it. It doesn't affect your application.


Have a great day,
TIC   Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信