Differences between iMX7 Sabre Rev B and Rev D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differences between iMX7 Sabre Rev B and Rev D

1,613 Views
brianpaiva
Contributor III

I have an MCIMX7D-SABRE RevB (SCH-28590 Rev B), but the only schematic that I can find is for Rev D(SCH-28590 Rev D).  Are there any major differences between the two and is there a Rev B schematic available?  I'm trying to get support for SDR104 SD Cards, but can't get it to work in 1.8V mode.

Labels (1)
3 Replies

1,435 Views
jan_spurek
NXP Employee
NXP Employee

Hello Brian,

all changes should be listed on the first page of the board schematic.

Best Regards,

Jan

1,435 Views
brianpaiva
Contributor III

Based on what I read, am I right in assuming that for SD1 the only way to support SDR104 is to set it in the fuses?

0 Kudos
Reply

1,435 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  NVCC_SD1 supply voltage is provided by the PMIC on the i.MX7 SABRE

design. This voltage is configured using SD_VSEL signal of the PMIC:

SD_VSEL is input from i.MX processor (GPIO1_IO08 on the SABRE) to select

VCC_SD regulator voltage. So, SD1 supply voltage is programmable.

   IMX7 GPIO1_IO08 default state is GPIO port, input, pulled down, therefore

just after reset NVCC_SD1 is 3 V. Customers cannot change it for SD1 boot,

but can modify the voltage after boot in OS.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply