Difference of DRAM_SDCLK in i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference of DRAM_SDCLK in i.MX6

2,288 Views
ko-hey
Senior Contributor II

Hi all

I have a question about difference of DRAM_SDCLK in i.MX6Q.

Is there any difference between DRAM_SDCLK0 and DRAM_SDCLK1 ?

I know that i.MX6Q has two DRAM_SDCLKs and it's for dual-channel DDR like LPDDR2.

So it's not difference when I use DDR3.

Am I correct ?

Ko-hey 

Labels (2)
Tags (2)
0 Kudos
Reply
4 Replies

1,974 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  generally the clocks are the same, but also, please 

take into account considerations, linked below.   

  https://community.nxp.com/thread/340453 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos
Reply

1,974 Views
nexy_sm
Contributor II

Hi all,

I would like to revive this question again. So what is the difference between this two clocks? I understand with 2 channel LPDDR there are two clocks that are used, but what if I have 4 DDR3 memory chips x16 bit and I would like to build x32 bit memory path with two times capacity. Can I use only one clock SDCLK0, or do I have to use also SDCLK1?

Thanks and cheers!

0 Kudos
Reply

1,974 Views
Yuri
NXP Employee
NXP Employee

Hello,

  it is possible to use any of both variants: SDCLK0 only, SDCLK0 and SDCLK1. 

Regards,

Yuri.

0 Kudos
Reply

1,974 Views
ko-hey
Senior Contributor II

Hi Yuri

Thank you for quick reply.

I'll check the link.

Ko-hey

0 Kudos
Reply