Difference between yocto setup distro version 1.6 and 1.7 .

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between yocto setup distro version 1.6 and 1.7 .

1,370 次查看
veeranjaneyulug
Contributor III

Hi

I have one doubt i used yocto versions 1.6 and yocto version 1.7 for two projects.But main thing is we  used kernel 3.0.35/3.10.17 versions for yocto 1.6 used .linux kernel version 3.14.28 for yocto 1.7 used.

May i know what is the main difference between 1.6 and 1.7 .is it depends on linux kernel version?

Thanks & Regards

veeranjaneyulu

标签 (5)
0 项奖励
回复
2 回复数

1,255 次查看
marcocavallini
Contributor V

Hi veeranjaneyulu,

generally speaking you should be able to replace the kernel version without problems keeping the same image created with older Yocto Project version. Consider that the YP version changes usually involve the GPU and/or graphical section so keep a coherent build system and environment is a best practice.

Distinti Saluti / Best Regards

--

Marco Cavallini | KOAN sas | Bergamo - Italia

Yocto Project Advocate

0 项奖励
回复

1,255 次查看
igorpadykov
NXP Employee
NXP Employee

Hi veeranjaneyulu

please look at

FSL Community BSP Release Notes 1.6 documentation

FSL Community BSP Release Notes 1.7 documentation

and post additional questions on

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复