Difference between the two USB ID pins?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Difference between the two USB ID pins?

跳至解决方案
3,795 次查看
adevries
Contributor V

Hello,

I'm planning to use 8M Mini's USB ports in OTG mode. I saw that both USB ports have 2 ID pins. For USB1, it is signal usb_id, located on pad USB1_ID [D22] and usb_otg_id, located on pad GPIO_IO10 [AD10]. Are these ID pins redundant? Or do they accomplish different things? Just trying to figure out if I need route one or both to the USB connector.

Thanks

标签 (1)
0 项奖励
回复
1 解答
3,607 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The two pin function are the same. Here if you use the usb in OTG Mode you can refer to our i.MX6 series board reference design. You can use the usb1_id, and you also can use the usb1_otg_id. If you are using the usb1_otg_id, you'd better use the usb1_id the same with the usb1_otg_id.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,608 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The two pin function are the same. Here if you use the usb in OTG Mode you can refer to our i.MX6 series board reference design. You can use the usb1_id, and you also can use the usb1_otg_id. If you are using the usb1_otg_id, you'd better use the usb1_id the same with the usb1_otg_id.

0 项奖励
回复
3,607 次查看
adevries
Contributor V

Hi Rita,

Thanks for the information. I'm a little confused by your last sentence, "If you are using the usb1_otg_id, you'd better use the usb1_id the same with the usb1_otg_id". Does that mean if I am using signal usb_otg_id (on pin AD10), then I must also use usb1_id (on pin D22)?

Thanks

0 项奖励
回复
3,607 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, and you need to pull up the usb1_id pin.

0 项奖励
回复
3,607 次查看
adevries
Contributor V

Hi Rita,

I'm still confused by this. Are you saying that I can use pin D22 to sense the USB ID signal, or I can use pin AD10 and pin D22 shorted together to sense the USB ID signal? Why couldn't I use pin AD10 by itself?

Also, can I use the internal pull-up resistors to pull the USB ID signal high?

Thanks

0 项奖励
回复