Difference between pf0100 and pf0200

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between pf0100 and pf0200

ソリューションへジャンプ
1,839件の閲覧回数
JHY
Contributor IV

I want to replace pf0100 with pf0200 in i.MX6DL boards.

Are they pin-to-pin compatible or need another work for PCB?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,644件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

MMPF0200 is MMPF0100 (pin compatible) minus SW1C and SW4, SW2=1.5A.

Since SW1C is absent in the PF0200, both VDDCORE and VDDSOC

are powered by the SW1AB regulator. Peripherals connected to the SW4

regulator in the original reference design can be powered by the SW2 regulator

when using the PF0200.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,645件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JHY

MMPF0200 is MMPF0100 (pin compatible) minus SW1C and SW4, SW2=1.5A.

Since SW1C is absent in the PF0200, both VDDCORE and VDDSOC

are powered by the SW1AB regulator. Peripherals connected to the SW4

regulator in the original reference design can be powered by the SW2 regulator

when using the PF0200.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信