Difference between QT on Linux and on Integrity RTOS?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Difference between QT on Linux and on Integrity RTOS?

跳至解决方案
1,712 次查看
maheshkumarkoda
Contributor III

Hallo,

I would like to know the difference between porting QT on Embedded Linux and on Integrity RTOS with Sabreauto board:

1). What are the compatible modules interfaced between Linux and QT framework?

for example : Wayland and X11?

2). How Integrity can be ported with QT?

Can Wayland , X11 be ported with integrity?

3). Is there any architectural diagram which explains Linux+QT port?

please provide if any.

Thanks,

Mahesh.

标签 (2)
0 项奖励
回复
1 解答
1,428 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

these are specific OS questions and may be posted on appropriate specialized forums like

http://qt-project.org/wiki/i.MX-6

Embedded Devices with Qt and the INTEGRITY RTOS - Qt Blog 

from hardware point of view, drivers are the same for these opearting systems

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,429 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

these are specific OS questions and may be posted on appropriate specialized forums like

http://qt-project.org/wiki/i.MX-6

Embedded Devices with Qt and the INTEGRITY RTOS - Qt Blog 

from hardware point of view, drivers are the same for these opearting systems

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复