Difference between QT on Linux and on Integrity RTOS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between QT on Linux and on Integrity RTOS?

ソリューションへジャンプ
2,304件の閲覧回数
maheshkumarkoda
Contributor III

Hallo,

I would like to know the difference between porting QT on Embedded Linux and on Integrity RTOS with Sabreauto board:

1). What are the compatible modules interfaced between Linux and QT framework?

for example : Wayland and X11?

2). How Integrity can be ported with QT?

Can Wayland , X11 be ported with integrity?

3). Is there any architectural diagram which explains Linux+QT port?

please provide if any.

Thanks,

Mahesh.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,020件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

these are specific OS questions and may be posted on appropriate specialized forums like

http://qt-project.org/wiki/i.MX-6

Embedded Devices with Qt and the INTEGRITY RTOS - Qt Blog 

from hardware point of view, drivers are the same for these opearting systems

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,021件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mahesh

these are specific OS questions and may be posted on appropriate specialized forums like

http://qt-project.org/wiki/i.MX-6

Embedded Devices with Qt and the INTEGRITY RTOS - Qt Blog 

from hardware point of view, drivers are the same for these opearting systems

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信