Difference between MCIMX6 and PCIMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Difference between MCIMX6 and PCIMX6

跳至解决方案
1,715 次查看
danielbujak
Contributor III

I've been developing on the MX6UL EVK with the PCIMX6G2CVM05AA, but am now looking to port to a custom PCB with the MCIMX6G2AVM07AA part on it. Where can I find information on the differences between these parts that I need to be aware of for the port?

标签 (1)
0 项奖励
回复
1 解答
1,488 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Danielbujak,

The PC in front of the par number refers to the part being a prototype sample. You can see more details on what the part number nomenclature means in figure 1 of the i.MX6UL Datahseet (link below):

http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf

I hope this helps!

Regards,

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,489 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Danielbujak,

The PC in front of the par number refers to the part being a prototype sample. You can see more details on what the part number nomenclature means in figure 1 of the i.MX6UL Datahseet (link below):

http://www.nxp.com/docs/en/data-sheet/IMX6ULCEC.pdf

I hope this helps!

Regards,

0 项奖励
回复
985 次查看
brian_21
Contributor I

For Special Qualification level, is the SC marked at the package body for this type of device?

0 项奖励
回复