Difference between Cortex A8 and A9 in power/performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between Cortex A8 and A9 in power/performance

1,131 Views
lyfsci
Contributor III

Hi Experts,

Is there any performance chart on the Linux kernel for the processor A8/A9 in terms of some metrics/parameters ?

Labels (1)
0 Kudos
Reply
1 Reply

973 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

suggest to look at power measurements for i.MX6,53 processors with A9/A8 cores.

AN4715 AN4715, i.MX 6Solo Power Consumption Measurement - Application Note

AN4270

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply