Difference between Cortex A8 and A9 in power/performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between Cortex A8 and A9 in power/performance

1,692件の閲覧回数
lyfsci
Contributor III

Hi Experts,

Is there any performance chart on the Linux kernel for the processor A8/A9 in terms of some metrics/parameters ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,534件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lyf

suggest to look at power measurements for i.MX6,53 processors with A9/A8 cores.

AN4715 AN4715, i.MX 6Solo Power Consumption Measurement - Application Note

AN4270

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信