Difference between 2-CPU and 4-CPU DRAM accesses?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between 2-CPU and 4-CPU DRAM accesses?

4,020件の閲覧回数
frank_vanhooft
Contributor III

We have an odd situation and would appreciate any suggestions. We've been building iMX8 Mini based boards for a while, running Yocto linux 5.15.32. Partnumbers:

CPU: MIMX8MM6DVTLZAA  (quad core iMX8 mini)

RAM: Micron MT53E256M32D2DS-053 AAT:B  (LPDDR4 1 GB, x32 wide, single chip)

Recently we've had a batch of boards that crash within minutes just when running the Linux OS. No application running, room temperature, but if we run 4 instances of memtester (one memtester running on each of the CPUs) we can get memtester errors. Looks like a simple RAM problem, right?

Here's the question. If we add the kernel argument:

nr_cpus=2

So now only 2 CPUs are used by the OS, then magically everything becomes stable. The boards will run for days. We can run 2 instances of memtester (one on each CPU) indefinitely, etc. 

There's only a single RAM interface, and a single RAM chip. So why would the RAM be stable for 2 CPUs and yet not for 4? What's the difference between 2 CPUs accessing RAM versus 4 CPUs accessing RAM (even when hammering RAM using multiple memtesters)?

Thanks.

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,896件の閲覧回数
frank_vanhooft
Contributor III

Two files attached. Both from the same board, but one with 4 CPUs and the other with nr_cpus=2. The 4 CPU log shows a crash. The 2 CPU runs OK. 

0 件の賞賛
返信

3,876件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @frank_vanhooft 

I checked the crash log and did same memory test with same kernel version. No such issue with 4 memtester instances.

From the crash log, the sync error is about page and cache swap. This could relate to DDR or kernel. Can you try more kernel version? like 5.15.71 ,6.1.55 and 6.6.3

0 件の賞賛
返信

3,936件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @frank_vanhooft 

Can you share test steps and logs?

Thanks

Zhiming

0 件の賞賛
返信