Diff between Imx6sl SoC revisions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Diff between Imx6sl SoC revisions

1,664 Views
sandeepajesh
Contributor III

Hi NXP,

We are facing some issue with hwclock utility on our new Imx6sl board. The only difference between two is SoC revision.

Older SoC revision:-MC IMX6L8DVN10AB BTJD1510

Newer SoC revision:- MC IMX6L8DVN10AA XAA1320

Please help.

Regards

Sandeep S

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

1,538 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sandeep

"AA" part is old 1.0 rev. not recommended for new designs, as shown on

Figure 1. Part Number Nomenclature—i.MX 6SoloLite i.MX6SL Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf

"AB" rev.1.2 latest silicon version of i.MX6SL. It addressed a few issues
one of which is ERR007926.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,538 Views
sandeepajesh
Contributor III

Hi Igor

Thanks for the information.Unfortunately we already have few boards with Rev1.0. 

Still I am not able to understand what exactly is causing hwclock --systohc to hang.

When I am executing this command on on Rev1.0 board system got hanged whereas its working on Rev1.2 board.[Same Binaries]

Regards

Sandeep S

0 Kudos
Reply

1,538 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sandeep

one can try to debug it using AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors

http://www.nxp.com/files/32bit/doc/app_note/AN4553.pdf 

~igor

0 Kudos
Reply

1,538 Views
sandeepajesh
Contributor III

Issue was with SoC revision. After upgrading to Soc version 1.2 hwclock is working fine.

0 Kudos
Reply