Device tree compatibility between iMX6ULL and iMX6ULZ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device tree compatibility between iMX6ULL and iMX6ULZ

1,477 Views
jupiter_hce
Contributor III

Hi,

Our iMX6 customization development was based on iMX6 EVK main board revision 700-28616 REV A1, SCH-28616 REV C2, MCU board revision 700-29364 REV A, SCH-29364 REA, the EVK processor is MCIMX6Y2DVM09AA of iMX6ULL, but we purchased MCIMX6Z0DVM09AB which is iMX6ULZ, the device tree is based on available imx6ullevk.conf and imx6ull-14x14-evk.dtb at time.

NXP developers have since added imx6ulz-14x14-evk.conf and imx6ulz-14x14-evk.dtb to meta-freescale for u-boot and kernel 5, what is the subtle device tree compatibility difference between imx6ullevk.conf, imx6ull-14x14-evk.dtb and imx6ulz-14x14-evk.conf,  imx6ulz-14x14-evk.dtb? Which one should be used?

Thank you.

Kind regards,

jh

 

 

 

0 Kudos
Reply
1 Reply

1,471 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jupiter

 

for i.MX6ULZ imx6ulz-14x14-evk.conf, imx6ulz-14x14-evk.dtb should be used,

difference between i.MX6ULL and i.MX6ULZ is described in AN12264

i.MX 6ULZ Migration Guide

 

Best regards
igor

0 Kudos
Reply