Device Tree file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Tree file

5,465件の閲覧回数
VinithNama
Contributor III

Hi Sir/Madam,

                     I'm working on imx8m mini EVK on Linux environment, I'm modifying the imx8mm-evk .dts file in the kernel-source/aarch/arm64/boot/dts/freescale location after modifying the file I'm building the dts file using bitbake –c menuconfig linux-imx after building the dts file, I'm generating the images using bitbake imx-image-full and copying the images to the sdcard when i'm booting the evk with this sdcard I'm unable to see the pin what i have modified in dts file.

0 件の賞賛
返信
3 返答(返信)

4,421件の閲覧回数
r_trivedi123
Contributor IV

Hi @VinithNama  ,

you can check either of any
1. DTBO is implemented which is overwriting your dts configuration
2. Check the md5sum of the actual generated dtb vs on board dtb
3. In U-boot check weather the dtbo is actually being taken into account while booting kernel using printenv command
4. Perhaps the same GPIO is being configured alternatively, the final config can be checked post booting /sys/kernel/debug/gpio ?

--
Rutvij Trivedi
Silicon Signals Pvt. Ltd.
[email protected]

--
Rutvij Trivedi

0 件の賞賛
返信

5,461件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

5,455件の閲覧回数
VinithNama
Contributor III

I have modified the device tree and added the dtb file in the u-boot time and booted the EVK board, when I'm exporting the gpio pins and checking the voltage levels using multimeter I'm unable to find the difference I have used Imx8m mini evk and the pin number is MX8MM_IOMUXC_SAI5_RXD1_GPIO3_IO22       0x19 and I have enable the sai5 group in dts file.

0 件の賞賛
返信