Device Driver (I/O Expander)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device Driver (I/O Expander)

2,158 Views
oprata
Contributor II

Hello Folks!
I am trying to develop a device driver for a I/O expander. The device that I use for it is PCF8574T from NXP. And I am using the IMX8MMEVK board to do it.

I wrote a device driver that it works fine - look the attached pcf8574t.tar.gz. But now I would like to map each GpIO of pcf8574t on sysfs over /sys/class/gpio. Does anybody has a tip about how can I do it?

Thanks in advance.

 

Labels (1)
0 Kudos
Reply
2 Replies

1,241 Views
Transidico
Contributor III
hello,
do you still have the code you made? I have the same problem, it would be very helpful.
Thanks
0 Kudos
Reply

2,147 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

You can see this reply https://forums.balena.io/t/gpio-mapping-on-variscite-board/80718 

 

BR

Zhiming

0 Kudos
Reply