Device Descriptor failed in imx6ul

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Device Descriptor failed in imx6ul

2,107件の閲覧回数
chandraevolute
Contributor V

Hi,

We got our custom board for production, we are using USB OTG port to flash the kernel, rootfs and uboot using mfgtool. 

When we change to download mode and connect the USB otg port to PC , it is throwing USB device discriptor failed in the device manager. Is there any solution for this problem. Using imx6ul processor and custom board. 

Regards,

Chandrasekhar

ラベル(3)
0 件の賞賛
返信
4 返答(返信)

1,963件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

how did you change and what the error information? pls give me more detailed information about your issue, when you connect board to PC, pls check if the PC can detect the board or not, pls share your operation steps.

0 件の賞賛
返信

1,963件の閲覧回数
chandraevolute
Contributor V

Using boot mode switches we are changing it to Download mode after that we are connecting USB otg 1 to PC(windows 10), then we are getting error (attached image check the highlighted in red). When we run mfgtool it is showing no device connected.

Capture.PNG

0 件の賞賛
返信

1,963件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

it seemsn the PC couldn't detect the board, you can try to install the driver or change to another PC, if your PC detect board, you should find it from "Human Interface Devices",

0 件の賞賛
返信

1,963件の閲覧回数
chandraevolute
Contributor V

We tried all the steps you have mentioned, still it is behaving the same way. We have 5 custom boards ,one board is working but rest of the boards are not working. Is there anything to be done on Hardware side??

0 件の賞賛
返信