Designing mx28 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Designing mx28 board

1,231 Views
pt
Senior Contributor I

Hi

I am using i.Mx281.

Which pin should be selected as SD0_WP?

In i.Mx287,SD0_WP is SSP1_SCK.But in 281,it is NC.

Can I use GPMI_RESETn as WP for ssp0?

Can I use any GPIO?

Regards

Parvathy

Labels (2)
Tags (1)
1 Reply

1,119 Views
igorpadykov
NXP Employee
NXP Employee

Hi Pt

yes in general one can use any GPIO for this

purpose. One can find example in

..linux/arch/arm/mach-mx28//device.c

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------