Deserializer in

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deserializer in

Jump to solution
1,720 Views
takashitakahash
Contributor III

When capturing iMX6D RGB565 format via the deserializer In

What is the signal assignment of the data bus.

Which corresponding bits to each bit of  data bus  to  R [5:00], G [5:01], b [5:00] ?

Labels (2)
0 Kudos
Reply
1 Solution
1,640 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
1,641 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,641 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

MIPI-CSI data bit placement is given in

sect.40.5.1 General/Arbitrary Data Reception

IMX6DQRM

as for CSI bit allocation one can look at

sect.4.11.10.1 IPU Sensor Interface Signal Mapping

IMX6DQCEC

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply