Hello,
I am looking to demonstrate a two-node CAN bus using the MCIMX8QM MEK + baseboard and another new CAN device I am designing. Before purchasing a MCIMX8-8X-BB baseboard, which supports CAN physical connections, I would like to confirm whether or not any of NXP's automotive pre-built demo images (for example, automotive-12.0.0_2.1.0_image_8qmek_car2) supports exercising any of the i.MX chip's CAN functionality by default or not? The CAN bus function is not a listed feature in the Android Release Notes [Rev. automotive-12.1.0_1.1.0 —15 December 2022, Table 2, Features] so presumably there is no demo image support, but please confirm?
Thanks.
Thank you @Rita_Wang. This info looks useful, however I am asking whether or not there is CAN functionality already in the NXP Android Automotive OS v12 pre-built demo images without building any code...? In other words, does changing the AAOS on-screen user controls for HVAC, for example, result in any iMX8QM CAN bus activity, etc.?
For the linux https://github.com/nxp-imx/linux-imx/blob/lf-5.15.52-2.1.0/arch/arm64/boot/dts/freescale/imx8qm-mek.... the can is enable.