Demo image for MCIMX6DL-SDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Demo image for MCIMX6DL-SDB

跳至解决方案
1,899 次查看
ko-hey
Senior Contributor II

Hi all

Could someone tell me the correct demo image for MCIMX6DL-SDB ?

My customer bought a MCIMX6DL-SDB and tried SD boot.

However, it didn't boot.

I checked the file in SD card and the SD card contain a following named file.

MX6DL-OBDS-REV-X8.exe

I think the file is wrong for booting.

Could you tell me the correct Linux and android image for MCIMX6DL-SDB ?

Ko-hey

标签 (4)
0 项奖励
回复
1 解答
1,752 次查看
bernhardfink
NXP Employee
NXP Employee

Hi Ko-hey,

the OBDS is a test suite for some (maybe all) i.MX boards (on-board diagnostic suite). It's used internally in NXP to bring up and test new development boards. In the i.MX28 times I know it was also intended to go out, to provide customers with a software which enables them to test their own i.MX based boards in an early project stage. For the i.MX6 I haven't seen packages like this going to the outside.

In my opinion, the SD card you got with this 6DL package is simply a mistake.

In the link from Joan Xie for the Linux software, you need to go to the "Board Support packages", click on "More" and then you can download the demo binaries of the latest release 4.1.15_2.0.0 (L4.1.15_2.0.0_MX6QDLSOLO, 2.2Gbytes). These demo binaries work for the Quad/Dual/Solo/DualLite.

Regards,

Bernhard.

在原帖中查看解决方案

4 回复数
1,752 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can download the mx6q demo image from nxp official website as below:

ANDROID (fucos on the "Board Support Packages"):

<Android OS for i.MX Applications Processors|NXP >

LINUX(fucos on the "Board Support Packages"):

<Embedded Linux for i.MX Applications Processors|NXP >

0 项奖励
回复
1,752 次查看
ko-hey
Senior Contributor II

Hi Joan Xie

Do you mean there has been a mistake ?

ko-hey

0 项奖励
回复
1,753 次查看
bernhardfink
NXP Employee
NXP Employee

Hi Ko-hey,

the OBDS is a test suite for some (maybe all) i.MX boards (on-board diagnostic suite). It's used internally in NXP to bring up and test new development boards. In the i.MX28 times I know it was also intended to go out, to provide customers with a software which enables them to test their own i.MX based boards in an early project stage. For the i.MX6 I haven't seen packages like this going to the outside.

In my opinion, the SD card you got with this 6DL package is simply a mistake.

In the link from Joan Xie for the Linux software, you need to go to the "Board Support packages", click on "More" and then you can download the demo binaries of the latest release 4.1.15_2.0.0 (L4.1.15_2.0.0_MX6QDLSOLO, 2.2Gbytes). These demo binaries work for the Quad/Dual/Solo/DualLite.

Regards,

Bernhard.

1,752 次查看
ko-hey
Senior Contributor II

Hi Bernhard Fink

Thank you !

Ko-hey

0 项奖励
回复