DeepViewRT Installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DeepViewRT Installation

1,572件の閲覧回数
Anonymous123
Contributor I

Hello Community,

I have a machine-learning model that I wanna deploy on the i.MX8MPlus processor, I installed the eIQ Toolkit 1.7.3 on my host machine and converted my model into the DeepViewRT format (.rtm).

My target hardware is the DEBIX Model A board, it has the NXP i.MX8MPlus processor, I flashed the board with the official DEBIX Ubuntu 22.04 image, and tried to install the DeepViewRT 2.44 found in:

<eIQ_Install_dir>/deepviewrt

 

And I got the following error (missed packages the DeepviewRT requires):

Selecting previously unselected package deepview-rt.
(Reading database ... 74436 files and directories currently installed.)
Preparing to unpack deepview-rt_2.4.44-aarch64-r0_arm64.deb ...
Unpacking deepview-rt (2.4.44-aarch64-r0) ...
dpkg: dependency problems prevent configuration of deepview-rt:
 deepview-rt depends on libopenvx-imx (>= 6.4.3.p4.2-aarch64); however:
  Package libopenvx-imx is not installed.
 deepview-rt depends on nn-imx; however:
  Package nn-imx is not installed.
 deepview-rt depends on onnxruntime; however:
  Package onnxruntime is not installed.
 deepview-rt depends on tensorflow-lite; however:
  Package tensorflow-lite is not installed.

dpkg: error processing package deepview-rt (--install):
 dependency problems - leaving unconfigured
Errors were encountered while processing:
 deepview-rt

 

Where I can get these missed packages from? or how would I get the DeepViewRT installed on my target hardware?

 

Kind regards,

0 件の賞賛
返信
1 返信

1,498件の閲覧回数
brian14
NXP TechSupport
NXP TechSupport

Hi @Anonymous123, 

This is an image provided by DEBIX and it seems that the machine learning layer is not included in the build image process and doesn’t support machine learning execution.
Please contact DEBIX support to correctly implement this package on this target.

Have a great day!

Best regards, Brian.

0 件の賞賛
返信