Decoding multiple H.264 streams with i.MX8M VPU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Decoding multiple H.264 streams with i.MX8M VPU?

2,367 次查看
martin_gisbert
Contributor I

Hi,

the i.MX8M's VPU features a 1080p60 H.264 decoder (up to high profile). Is it possible to use this VPU to decode *multiple* streams with a lower frame rate, e.g. 4 streams of 15 fps each? Or possibly even more streams with a lower resolution and/or profile, like maybe 6 x 720p15 (low profile)?

Thanks,

Martin

标记 (3)
0 项奖励
回复
3 回复数

2,133 次查看
marcelbässler
Contributor III

Hi,

I got the same question.

2to4 IP Streams from Camera and it should be shown on monitor.

Is it possible with i.MX8M or i.MX8MQM?

0 项奖励
回复

2,133 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Martin,

Yes its possible, MX8M its up to

  • 4K @ 60fps with High Dynamic Range:
    - h.265
  • 4K @ 30fps
    - h.264

How to use dual display on i.MX8 including 4k decoding - i.MXDev Blog 

Regards

0 项奖励
回复

2,133 次查看
martin_gisbert
Contributor I

Thanks for the response, but I guess my question was not clear enough, so let me get more specific:

My customer is using several IP cameras and their capture should be shown on a display. So there are 2-4 H.264 streams that have to be decoded.

Is this possible with the i.MX8M VPU?

Thanks,

Martin

0 项奖励
回复