Decoder issue with i.MX8 EVK platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Decoder issue with i.MX8 EVK platform

1,120 Views
sunithas
Contributor I

 I am trying to test i.MX8 hardware decoder using the package downloaded from [https://github.com/Freescale/libimxvpuapi] Package compilation failed for i.MX8 EVK platform because of libvpu.so library not found Where can i get source code for libvpu or libvpu.so ??

Regards,

Sunitha

Tags (2)
0 Kudos
Reply
1 Reply

1,000 Views
art
NXP Employee
NXP Employee

The generic libvpu library of i.MX6 family processors cannot be used with i.MX8/i.MX8M processors since the video processing hardware of these processor families is significantly different. Also, the VPU libraries are not distributed by NXP in source code form since all video processing hardware of i.MX series processors are the IP-cores of various 3rd party vendors, so, NXP has no rights to distribute the source code. The corresponding pre-compiled binary libraries can be found within various BSP distributions for corresponding processor families.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply