Debugging tools (JTAG)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging tools (JTAG)

2,789件の閲覧回数
JohnBirch
NXP Employee
NXP Employee
OK, who has used what tools successfully, including kernel level debuggers?
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,358件の閲覧回数
sinanakman
Senior Contributor III

Abatron's BDI3000 (I use those for all my platforms : mpc8379, mpc8323, mpc5125, imx28, imx53, imx6,  p2020, p2040 etc)

0 件の賞賛
返信

2,358件の閲覧回数
positron
Fresh Out Contributor

This is the first time I'm hearing about Jtagkey2p. I'm quite familiar with JLINK. What problems do you face with JLINK. May be you can post that to the JLINK forums. I don't know whether ULINK2 supports Linux kernel debugging.

For user-space : gdb over ethernet is fine.

For kernel-space: you must need a perfectly working debugger to focus on porting. I'm not sure which JTAG is cheap. May be you can take the help of google.

0 件の賞賛
返信

2,358件の閲覧回数
positron
Fresh Out Contributor

Jose, It is quite tough to debug kernel/drivers effectively using an ethernet connection, especially if you want to debug a crash right at the kernel entry point. So, the best choice would be a JTAG debugger.

What's your intention of debugging anyway? Just for learning or want to port something on a custom hardware?

0 件の賞賛
返信

2,358件の閲覧回数
myke_predko
Senior Contributor III

Hey John,

 

I'm partial to using GDB to cross-debug via Ethernet (as described in AN3870). 

 

With the Ethernet connection, I can also use TFTP to download built apps into the NAND Flash of the i.MX which makes the data path relatively simple. 

 

myke

0 件の賞賛
返信