Debug Thread Running

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug Thread Running

1,670件の閲覧回数
hkhunkim
Contributor I

Hello, I am trying to use atwilc1000-sd as wifi sd-card to imx6qdlsabreauto board.

In short, I was able to insert device driver with "insmod wilc-sdio.ko" command and firmwares are also included.

This could be checked with belows. (with 'ifconfig wlan0 up' command)

wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_mac_open]MAC OPEN[d913b800] wlan0
power up request for already powered up source Wifi
Device already up. request source is Wifi
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_init_host_int]Host[d913b800][d8c4c6c0]
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_mac_open]*** re-init ***
wilc_sdio mmc0:0001:1 wlan0: INFO [wlan_init_locks]Initializing Locks ...
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_init]Initializing WILC_Wlan
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_initialize]WILC Initialization done
wilc_sdio mmc0:0001:1 wlan0: INFO [init_irq]IRQ request succeeded IRQ-NUM= 129 on GPIO: 91
wilc_sdio mmc0:0001:1 wlan0: INFO [wlan_initialize_threads]Initializing Threads ...
wilc_sdio mmc0:0001:1 wlan0: INFO [wlan_initialize_threads]Creating kthread for transmission
wilc_sdio mmc0:0001:1 wlan0: INFO [wlan_initialize_threads]Creating kthread for Debugging
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_get_firmware]Detect chip WILC1000
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_get_firmware]loading firmware mchp/wilc1000_wifi_firmware.bin
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_get_firmware]WLAN firmware: mchp/wilc1000_wifi_firmware.bin
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_firmware_download]Downloading Firmware ...
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_firmware_download]Downloading firmware size = 134964
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_firmware_download]Offset = 119660
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_firmware_download]Offset = 134964
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_firmware_download]Download Succeeded
wilc_sdio mmc0:0001:1 wlan0: INFO [linux_wlan_start_firmware]Starting Firmware ...
wilc_sdio mmc0:0001:1 wlan0: INFO [linux_wlan_start_firmware]Waiting for FW to get ready ...
wilc_sdio mmc0:0001:1 wlan0: INFO [linux_wlan_start_firmware]Firmware successfully started
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_wlan_initialize]WILC Firmware Ver = WILC_WIFI_FW_REL_15_01_RC3 Build: 9792
wilc_sdio mmc0:0001:1 wlan0: INFO [linux_wlan_init_test_config]Start configuring Firmware
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_mac_open]Mac address: fa:f0:05:f1:41:fb
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Setting mcast List with count = 0.
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Enable mcast filter retrive directed pkts only
wilc_sdio mmc0:0001:1 wlan0: INFO [set_power_mgmt] Power save Enabled= 1 , TimeOut = -1
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Setting mcast List with count = 1.
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[0]: 1:0:5e:0:0:1
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Setting mcast List with count = 2.
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[0]: 1:0:5e:0:0:1
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[1]: 33:33:0:0:0:1
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Setting mcast List with count = 3.
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[0]: 1:0:5e:0:0:1
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[1]: 33:33:0:0:0:1
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[2]: 33:33:ff:f1:41:fb
root@imx6qdlsabreauto:/usr/src/kernel# wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Setting mcast List with count = 4.
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[0]: 1:0:5e:0:0:1
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[1]: 33:33:0:0:0:1
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[2]: 33:33:ff:f1:41:fb
wilc_sdio mmc0:0001:1 wlan0: INFO [wilc_set_multicast_list]Entry[3]: 33:33:0:0:0:fb
wilc_sdio mmc0:0001:1 wlan0: INFO [debug_thread]*** Debug Thread Running ***
wilc_sdio mmc0:0001:1 wlan0: INFO [debug_thread]*** Debug Thread Running ***
wilc_sdio mmc0:0001:1 wlan0: INFO [debug_thread]*** Debug Thread Running ***

wilc_sdio mmc0:0001:1 wlan0: INFO [debug_thread]*** Debug Thread Running ***

However, as you could see, it has been stuck in wilc_set_multicast_list.

Can anyone tell me what to do?

Belows are my local.conf and wpa_supplicant.conf

- local.conf

MACHINE ??= 'imx6qdlsabreauto'
DISTRO ?= 'fslc-xwayland'
PACKAGE_CLASSES ?= "package_deb package_rpm"
EXTRA_IMAGE_FEATURES ?= "debug-tweaks package-management dbg-pkgs tools-sdk tools-debug"
CORE_IMAGE_EXTRA_INSTALL += "dhcp-client"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"
BB_DISKMON_DIRS ??= "\
    STOPTASKS,${TMPDIR},1G,100K \
    STOPTASKS,${DL_DIR},1G,100K \
    STOPTASKS,${SSTATE_DIR},1G,100K \
    STOPTASKS,/tmp,100M,100K \
    ABORT,${TMPDIR},100M,1K \
    ABORT,${DL_DIR},100M,1K \
    ABORT,${SSTATE_DIR},100M,1K \
    ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-native = " sdl"
PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
CONF_VERSION = "1"

CORE_IMAGE_EXTRA_INSTALL += " firmware-imx linux-firmware wireless-tools i2c-tools packagegroup-base wpa-supplicant"

IMAGE_INSTALL_append += " hostapd make wget apt tslib iproute2 gcc dhcpcd evtest kernel-devsrc ncurses iptables iw net-tools ethtool pciutils modutils-initscripts kernel-modules"

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"
IMAGE_ROOTFS_EXTRA_SPACE = "10048576"
IMAGE_FSTYPES += "wic wic.gz"

INHERIT+="toaster buildhistory"

- wpa_supplicant.conf

ctrl_interface=/var/run/wpa_supplicant

ctrl_interface_group=0

update_config=1

network={ ssid="MYSSID" psk="MY-SECURE-PASSKEY" proto=RSN key_mgmt=WPA-PSK }

0 件の賞賛
返信
1 返信

1,365件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

you should check the wifi driver

0 件の賞賛
返信