Debug IMX6QuadSabre SD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug IMX6QuadSabre SD

1,220件の閲覧回数
ailtonlopes
Contributor III

Hi, id like to know if there's any way to debug the imx6q board without the need of the ARM DSTREAM using baremetal application. 
Kind Regards.

Ailton Lopes

0 件の賞賛
返信
1 返信

1,134件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Generally the following summary link contains information about recommended tools.
Please look at sections "Hardware Development Tools" and  "Software Development Tools".
     
i.MX Software|NXP

In addition to  ARM DSTREAM customers can consider  Lauterbach Trace32
and Segger J-link. Please refer to tool providers for more details.

http://www.lauterbach.com/frames.html?powertools.html 

Debugging using Segger J-Link JTAG - Boundary Devices 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信