Debian on i.mX287

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debian on i.mX287

1,510 次查看
carloventrella
Contributor I

Hi, all.

I'm very newbie. Is it possibile to install debian within this processor?

If not, which processor supports it?

UPDATE

The board in issue is this: PLC operator panel, PLC with HMI

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,314 次查看
fabio_estevam
NXP Employee
NXP Employee

Yes, it is possible.

Here is a tutorial for mx23 that you can refer to and adapt it to mx28:

https://eewiki.net/display/linuxonarm/iMX233-OLinuXino

Regards,

Fabio Estevam

0 项奖励
回复

1,314 次查看
carloventrella
Contributor I

Thank you Fabio.

I updated the question with the spec of the board and maybe I've too low memory to mount debian.

However, what do you mean with 'adapt it to mx28'? Should I change something?

For example in the section Bootloader -> patches I see:

wget -c https://rcn-ee.com/repos/git/u-boot-patches/v2015.10-rc3/0001-mx23_olinuxino-uEnv.txt-bootz-n-fixes.patch

patch -p1 < 0001-mx23_olinuxino-uEnv.txt-bootz-n-fixes.patch

That seems to be specific for mx23 .. isn't it?

0 项奖励
回复

1,314 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Sure it is possible,  in fact we have an UBUNTU BSP for the i.MX28EVK that you find in the following link, and since UBUNTU it is a distro from Debian, there is no limitation on the usage of Debian with any of the i.MX

i.MX287 Processors|Dual Ethernet|Freescale

0 项奖励
回复