Dear I.MX community developres

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dear I.MX community developres

2,018 Views
saida
Contributor II

hi all this is saida

i am starting design based i.mx processor

i have some doughts

1. can i place solo processor on Dual lite based evalution board which i have taken reference for design

2. in dual lite can i enable only one core for processing and single DDR is sufficient or not

3. is two cores can share a single DDR

thank you in advance

Labels (2)
0 Kudos
Reply
3 Replies

1,854 Views
igorpadykov
NXP Employee
NXP Employee

Hi saida

yes, one can place solo processor on Dual lite based evalution board.

In dual lite one can enable only one core for processing, single DDR is sufficient.

Two cores can share a single DDR.

Also it may be useful to look at AN4397

Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,854 Views
saida
Contributor II

First of all i thank mr Igor for his valuable reply

i am new bee for i.mx6 DualLite processor and want to design new

custom made board

my requirement is i want to start a new board and ready to purchase

tools everything that processor needs

Design:

Host is Windows based PC

1. i want to design a new custom made board

2. i have to port U-boot for my board where i can store in Flash

3. i want to develop a non OS or OS approach code for my application

4. what are the IDE tools for code,compile.build,downloading,debugging

and flash programming

5. also i want hardware emulator(ICE) for my board .

kindly help me in this regard

Regards & Thanks

Saida Safavath

0 Kudos
Reply