Data Encryption Decryption over LittleFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Data Encryption Decryption over LittleFS

ソリューションへジャンプ
3,770件の閲覧回数
kotalamit
Contributor III

Hi,

In our application based on IMXRT1170, we plan to have LittleFS over the Flash Memory. Since we plan to have user data being saved to be encrypted and decrypted as a routine feature, want to check if using the Inline Encryption Engine be an appropriate utility?  Any other insights/suggestion will also be helpful.

 

Regards,

Amit Kotal

ラベル(3)
0 件の賞賛
返信
1 解決策
3,719件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @kotalamit ,

Yes, this is because flash programming use IP command, it doesn't use AHB bus. IEE can't help. You have to use IEE region 0 or other peripherals or software to encrypt the plaint text first, then do like the demo.

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,746件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @kotalamit ,

I think it is possible. You can refer to the iee_apc_cm7 project in the SDK demo folder.

 

Regards,

Jing

0 件の賞賛
返信
3,736件の閲覧回数
kotalamit
Contributor III

Hi @jingpan 

Thanks for the reply. With reference to the example, you mentioned; in that there is only decryption of the data stored in flash. No encryption for the flash data storage.

Additionally, in reference manual section 7.10 it is mentioned as decrypting only over Flex SPI.

 

Regards,

Amit K

0 件の賞賛
返信
3,720件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @kotalamit ,

Yes, this is because flash programming use IP command, it doesn't use AHB bus. IEE can't help. You have to use IEE region 0 or other peripherals or software to encrypt the plaint text first, then do like the demo.

 

Regards,

Jing

0 件の賞賛
返信